2023-10-28 12:20 AM
Hello together,
does anyone know how I can implement multiple USB device classes on a STM32?
I want to use the CDC so a VCP and the DFU class so I can communicate with my chip and drive an update if needed. I am working with a STM32L452RE.
It must be possible, it is the standard functionality of every ST-Link V2/V3 debugger that exists.
In the CubeMx you can not set this, is that documented somewhere? Unfortunately I haven't found anything yet.
Thanks for your assistance!
Solved! Go to Solution.
2023-10-28 04:24 AM
The keyword is "composite device". Search for it and you'll find enough information.
2023-10-28 04:24 AM
The keyword is "composite device". Search for it and you'll find enough information.
2023-10-29 05:21 PM
you can download the L4 cube firmware in st.com and there is USB middleware in stm32cube_fw_l4\Middlewares dir.
2023-10-30 01:19 AM
This was the right key word. Found this which looks nice: I-CUBE-USBD-Composite
2024-01-18 10:26 PM
Hi,
it is a shame that CubeMX does not support a combination of several device classes. After one day of searching examples i found a "software pack" for CubeMX:
alambe94/I-CUBE-USBD-Composite: Create STM32 USB Composite devices with ease. (github.com)
ST, please support this project and promote it, so we all can save lifetime!
I use:
CubeMX 6.10.0
CubeIDE 1.14.0
Processor: STM32F407VGT
2024-01-21 10:47 PM
Yeah, same thing as I posted.
But now I can say, the question was useless in my case, since when I jump into bootloader application from running application it switches the usb device class from CDC to DFU. So no special function is required in my case