cancel
Showing results for 
Search instead for 
Did you mean: 

How can i test Low power current consumption on Nucleo-4R5ZI development kit?

MBhar
Associate II

Please suggest code and setup to test all low power modes supported by the STM32L4 controller series and Nucleo-4R5ZI development kit

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
T J
Lead

If you had a well known resistor, say 2.00 ohms(1% or 0.1%) and put that in series from the power supply to the board, then measure the voltage across it...

ie V=IR,

I = V/R

use a multi meter...

MBhar
Associate II

Hi Nick,

Thank you for the response, i am unable to test Low power sleep mode code on the Nucleo-4R5ZI development kit. I am using kit and switch as mentioned.

I just want to know is anything else required to test low power mode code?