2020-02-12 6:08 AM
Hi all, I'm using a stm32f10x connected to a CANalyzer in order to verify the integrity of the CAN bus. The implemented process is simple, I have transmitted a CAN trace ( 11 bit ID + 8 bytes of DATA ) to the CANalyzer and it responses automatically with another CAN trace ( different ID and DATA values, but still using 11 bit ID ). The CAPL script is correct and the trace is received properly through CAN1, but only if I DISABLE the FIFO0 pending bit interruption.
// Enable CAN interrupt
CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE); // Q: If I DISABLE it, my code works.
How can I handle this interruption ?
I checked with :
CAN_GetITStatus(CAN1, CAN_IT_FMP0);
and it triggered in :
/* Check CAN_RF0R_FMP0 bit */
itstatus = CheckITStatus(CANx->RF0R, CAN_RF0R_FMP0);
being the status :
if ((CAN_Reg & It_Bit) != (uint32_t)RESET)
{
/* CAN_IT is set */
pendingbitstatus = SET; // This one. How can I lower this flag ?
}
--- My CAN configuration code is this one : ---
void CAN_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
CAN_InitTypeDef CAN_InitStructure;
CAN_FilterInitTypeDef CAN_FilterInitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOA, ENABLE);
/* Configure CAN pin: RX */
GPIO_InitStructure.GPIO_Pin = RX_CAN_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(CAN_GPIO, &GPIO_InitStructure);
/* Configure CAN pin: TX */
GPIO_InitStructure.GPIO_Pin = TX_CAN_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(CAN_GPIO, &GPIO_InitStructure);
/* 'WKUP_EXP' */
GPIO_InitStructure.GPIO_Pin = WAKEUP_CAN_PIN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Init(CAN_WAKEUP_GPIO, &GPIO_InitStructure);
/* CANx Periph clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);
/* CAN register init */
CAN_DeInit(CAN1);
CAN_StructInit(&CAN_InitStructure);
/* CAN cell init */
CAN_InitStructure.CAN_TTCM = DISABLE;
CAN_InitStructure.CAN_ABOM = DISABLE;
CAN_InitStructure.CAN_AWUM = DISABLE;
CAN_InitStructure.CAN_NART = DISABLE;
CAN_InitStructure.CAN_RFLM = DISABLE;
CAN_InitStructure.CAN_TXFP = DISABLE;
CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;
/* CAN Baudrate = 125kBps*/
CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;
CAN_InitStructure.CAN_BS1 = CAN_BS1_3tq;
CAN_InitStructure.CAN_BS2 = CAN_BS2_5tq;
CAN_InitStructure.CAN_Prescaler = 32;
CAN_Init(CAN1, &CAN_InitStructure);
/* CAN filter init */
CAN_FilterInitStructure.CAN_FilterNumber = 0; // Filter 0 for CAN1.
CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;
CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit;
CAN_FilterInitStructure.CAN_FilterIdHigh = 0x206 << 5; // This ID is the received one.
CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x7FF << 5; // Check all bits form ID.
CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;
CAN_FilterInitStructure.CAN_FilterFIFOAssignment = CAN_FIFO0; // Use FIFO0.
CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;
CAN_FilterInit(&CAN_FilterInitStructure);
NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 5;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
// Enable CAN interrupt
CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE); // If I DISABLE it, my bellow code works.
}
--- My CAN Write then Read code is this one : --- ( Its a function returning the received CAN struct from CANalyzer using as input a predefined CAN struct )
CanMsg_t FwMr13_SendCanMsg(const CanMsg_t *Msg)
{
CanTxMsg TxMessage;
CanRxMsg RxMessage;
uint8_t TxMailBox;
uint8_t TxStatus;
CanMsg_t RxMsg;
ITStatus CANinterruptStatus;
TxMessage.IDE = CAN_Id_Standard;
TxMessage.StdId = Msg->Id;
TxMessage.DLC = Msg->Dlc;
memcpy(TxMessage.Data ,Msg->Data , 8);
TxMessage.RTR = CAN_RTR_Data;
TxMailBox = CAN_Transmit(CAN1, &TxMessage); // Transmit through CAN1.
TxStatus = CAN_TransmitStatus(CAN1, TxMailBox); // TxStatus is Ok.
CAN_CancelTransmit(CAN1, TxMailBox);
CANinterruptStatus = CAN_GetITStatus(CAN1, CAN_IT_FMP0); // Here triggers.
CAN_Receive(CAN1, CAN_FIFO0, &RxMessage); // Read CAN1.
RxMsg.Id = RxMessage.StdId;
RxMsg.Dlc = RxMessage.DLC;
memcpy(RxMsg.Data, RxMessage.Data, 8);
if(CAN_MessagePending(CAN1, CAN_FIFO0) != 0 )
CAN_FIFORelease(CAN1, CAN_FIFO0);
CAN_GetLastErrorCode(CAN1);
return RxMsg;
}
Thanks in advance,