How can I disable a I2S module ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-18 6:13 AM
I am using cube mx for my design and I have some peripherals (ADC, Timer, I2S2, I2S3). I am making streaming by usb of some of them.
I want to stoop i2s modules when i am not using it becouse affect to other modules sampling rate.
By default Cubemx make this:
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
MX_TIM2_Init();
MX_ADC1_Init();
MX_TIM3_Init();
MX_TIM1_Init();
MX_I2S2_Init();
MX_I2S3_Init();
/* USER CODE BEGIN 2 */
And I am trying to make this
witch(mode_audio){
case 1:
HAL_TIM_Base_Start_IT(&htim2);
break;
case 2:
__HAL_I2S_DISABLE(&hi2s2);
__HAL_I2S_DISABLE(&hi2s3);
HAL_ADC_Start_DMA(&hadc1, (uint32_t *)dmaBuffer, CH_BUFFERSIZE);
HAL_TIM_OC_Start (&htim1,TIM_CHANNEL_1);
case 3:
// Inializate both DMA
HAL_I2S_Receive_DMA(&hi2s2,(uint16_t *)data_i2s2,I2S_BUFFERSIZE);
HAL_I2S_Receive_DMA(&hi2s3,(uint16_t *)data_i2s3,I2S_BUFFERSIZE);
break;
but __HAL_I2S_DISABLE(&hi2s2); andHAL_I2S_DMAStop(&hi2s2) do not work.
Any idea. I want to stop the I2s module
Thanks for all kind regards, TC
- Labels:
-
ADC
-
I2S
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-18 6:33 AM
Hi again , that does not work
HAL_NVIC_DisableIRQ(DMA1_Stream3_IRQn);
HAL_NVIC_DisableIRQ(DMA1_Stream0_IRQn);
__HAL_I2S_DISABLE(&hi2s2);
__HAL_I2S_DISABLE(&hi2s3);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-18 7:00 AM
Which STM32?
What is "does not work"? What are exactly the symptoms, and how are they different from what you expect?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-18 7:08 AM - edited 2023-11-20 7:48 AM
Hi, the problem it is that there i a overstress in the process and the output is not correctly genrate or both module write inide the ame buffer.
Both module are writing in the same buffer so I2S is not stopped.
We can see that becouse hi and low signal are continuous. The higher part of the signal is from adc and the lower for i2s module. So I2S is not topped.
And this is the behaviour comment
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
MX_TIM2_Init();
MX_ADC1_Init();
MX_TIM3_Init();
MX_TIM1_Init();
//MX_I2S2_Init();
// MX_I2S3_Init();
In that case all signal came from ADC.
Thansk for your fast response.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-18 7:14 AM
It is for Stm32F401
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-18 7:31 AM
I don't quite understand what those pictures display.
Do you use I2S as receivers? Maybe you want to manually clear the I2S buffers after disabling them.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-18 7:42 AM
Ok, that pictures display 4 adc channel sampling at 48Khz for analog mics.
I can switch between I2S to Analog mics.
But if i use cubemx both modules are activated. Both DMA, from ADC (4channels) and for I2S3 and I2S2 tranfer info for same buffer.
If I stop I2S2 and I2S3 i think that only info form ADC dma must be transfer by streaming to pc.
I am using
HAL_NVIC_DisableIRQ(DMA1_Stream3_IRQn);
HAL_NVIC_DisableIRQ(DMA1_Stream0_IRQn);
for stop the DMA and
__HAL_I2S_DISABLE(&hi2s2);
__HAL_I2S_DISABLE(&hi2s3);
for stop the module and they did not stop. I can know this becoue a break point is in the DMA interrupt for I2S2 and I2S3 transfer and it stop there.
void DMA1_Stream0_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Stream0_IRQn 0 */
/* USER CODE END DMA1_Stream0_IRQn 0 */
HAL_DMA_IRQHandler(&hdma_spi3_rx);
/* USER CODE BEGIN DMA1_Stream0_IRQn 1 */
/* USER CODE END DMA1_Stream0_IRQn 1 */
}
/**
* @brief This function handles DMA1 stream3 global interrupt.
*/
void DMA1_Stream3_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Stream3_IRQn 0 */
/* USER CODE END DMA1_Stream3_IRQn 0 */
HAL_DMA_IRQHandler(&hdma_spi2_rx);
/* USER CODE BEGIN DMA1_Stream3_IRQn 1 */
/* USER CODE END DMA1_Stream3_IRQn 1 */
}
I try to use
#define __HAL_I2S_DISABLE( __HANDLE__) ((__HANDLE__)->Instance->I2SCFGR &=(uint16_t)(~SPI_I2SCFGR_I2SE))
I supposed that DMA must be stopped before stop I2S module but that not works.
This could be other option.
#define __HAL_I2S_DISABLE_IT( __HANDLE__, __INTERRUPT__ ) ((__HANDLE__)->Instance->CR2 &=(uint16_t)(~(__INTERRUPT__)))
But this option allow disable the interrupt but the module will be actived unnecessarily.
Could you suggest what would you do if you wanted to stop module I2S2 started by cubemx?
I know the logical thing to do is not to initialise it but I don't want to delete the cubemx configuration to keep the ioc file as documentation.I deactivate the modules within the code.
If all works well, the buffer should be overwritten by the adc's DMA, since it only has 192 samples 48*4 with a conversion trigger frequency through tim1 every 1/1khz
In fact when I comment on the Cubemx startup for is2 and i2s3 everything works as expected as shown in the graphs in the previous post.
Yes I2S2 modules works as reciver.
Kind regards, TC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-03 12:15 PM
Hello @Tomás Cabeza,
Have you tried to disable it using HAL_I2S_DMAStop() or HAL_I2S_DeInit(). This could be other option worth to try.
Hope this helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.