cancel
Showing results for 
Search instead for 
Did you mean: 

hidden pins in STM32L0 CAD Symbol and Footprint files

YFuku.3
Associate III

I downloaded "STM32L0 CAD Symbol and Footprint files", open STM32L0x1KUF6.bxl, and converted it to .lbr Eagle CAD file. I opened the file in Eagle and realized that some pins(No.1,5,17) are hidden. why? I'm a beginner of Eagle

1 REPLY 1
MFRIS
Associate

Hello,

This type of component are composed in many parties. I don't know Eagles, but for example in Altium designer, I see two parts. The first part is with all I/O pins, and the second part is dedicated to power pins with VDD (pins 1,17) and VDDA (pin 5).

So, from my point of view, I think there is a window in Eagles, from which you can select the part you want to see.

Best regards