cancel
Showing results for 
Search instead for 
Did you mean: 

Programming STM32F401RET6 WITHOUT Nucleo board

CMead
Associate

I'm trying to find how to program the STM32F401RET6 MCU on a standalone PCB without the development board. The datasheet specifies using JTAG for debugging but does not specify that this could be used for initial programming too.

Could anyone help me find this information?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Yes programmable via JTAG/SWD interface pins, and an external/stand-alone ST-LINK, or similar JTAG Pod, ie Segger J-Link, etc.

Device typically also programmable using the System Loader (BOOT0=High) via USART or USB, etc.

See AN2606 and related documentation.

https://www.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/12/1e/40/0c/CD00167594.pdf/files/CD00167594.pdf/jcr:content/translations/en.CD00167594.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..