cancel
Showing results for 
Search instead for 
Did you mean: 

Hi there, I’m using an STM32L432 and I’m trying deep sleep with mbed RTOS. Using tickless mode I've been able to set deep sleep at 700uA usage. However, using threads increases the current to 3mA, normal sleep uses 5mA. What has caused the increase?

GRing.1
Associate II
 
1 REPLY 1
Bruno_ST
ST Employee

Hi @GRing.1​ 

Question linked to mbed RTOS.

BR,

Bruno

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.