cancel
Showing results for 
Search instead for 
Did you mean: 

안녕하세요 100Mhz 50% 듀티 PWM�?� 만들고�? 합니다. datasheet �? STM32H723xE/G block diagram �?� 보면 최대 138Mhz가 �?�다고 하는�?� PWM 파형으로 100Mhz 정�?� PWM 출력�?� 가능할까요 ?

SLee.8
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Bruno_ST
ST Employee

Hello @SLee.8​ ,

I will answer in english if you don't mind ;-). Yes the datasheet STM32H723 Tables 54 or 55 (respectively HSLV = OFF or ON) the limit in frequency of the IO ports depending of the load C.

Speed=11 select the maximum speed (maximum consumption).

The max operating frequency of the PWM though the timers is in "6.3.35 Timer characteristics" (details by timers in 3.31 Timers and watchdogs)

BR,

Bruno

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.