2021-05-23 8:13 PM
For OSC i am using 32.768khz and caps 10pF, but output is not coming. so please give me suggestions for hardware & software chages to work 32.768khz clock work.
2021-05-23 8:30 PM
What's the crystal part# ? Is it a 6, 9 or 12 pF crystal? Capacitors calculated per Application Note?
Should be able to walk-in the LSE enable via RCC/PWR register bits. Should be able to route the LSE clock via MCO1 / PA8 to measure without loading the circuit.
2021-05-23 8:38 PM
Hi Tesla,
Thanks for your response.
Crystal Part: CM315D-32.768KDZC-UT
Please share cap values to above crystal part for hardware changes.
2021-05-23 10:10 PM
Surely you should be able to run your own numbers?
I'd perhaps try 4.7pF or 5.1pF
Run a simple application to enable the clocks, and plumb the output to the MCO1 (PA8) pin.
2021-05-23 10:15 PM
Thank you, Tesla.
I will test and come back to you.
2021-05-24 3:49 AM
@Hi Tesla,
I attached scope image of PA8 output, but signal is in square wave and F= 32.72khz coming instead of 32.768khz.
Need some more changes required for exact clock 32.768khz ?
2021-05-26 2:51 AM
I am also using STM32F779 MCU in that OSC(RTC) clock is not behaving well please guide me the reason of this issue you can see here the details in my account.
2021-05-26 5:38 AM
2021-05-26 5:39 AM
2021-05-26 5:40 AM