2022-03-27 10:24 PM
A hex file generated from STM32F746ZGT6 is it compatible with STM32F756ZGT6?
Solved! Go to Solution.
2022-03-28 01:18 AM
Hello,
The two devices have the same memory mapping and same features except STM32F756 features a Crypto hardware acceleration. So yes, you can load a hex file generated for STM32F746ZGT6 to STM32F756ZGT6 device.
2022-03-28 01:18 AM
Hello,
The two devices have the same memory mapping and same features except STM32F756 features a Crypto hardware acceleration. So yes, you can load a hex file generated for STM32F746ZGT6 to STM32F756ZGT6 device.
2022-03-28 02:17 AM
thank you so much...!
2022-03-28 02:35 AM
You're welcome. Please close this thread by clicking "Select as best" in the answer.
2022-03-28 06:18 AM
Perhaps mark the actual answer to the question as the best, rather than your response.