2011-09-15 10:57 PM
just tryin to send PE.06 high but its not workin. is it my sourcecode? IT DOES compile without error or warnings.
#include ''stm32f10x_lib.h''
void Clk_Init (void)
{ // 1. Clocking the controller from internal HSI RC (8 MHz) RCC_HSICmd(ENABLE); // wait until the HSI is ready while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET); RCC_SYSCLKConfig(RCC_SYSCLKSource_HSI); // 2. Enable ext. high frequency OSC RCC_HSEConfig(RCC_HSE_ON); // wait until the HSE is ready while(RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET); // 3. Init PLL RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_9); // 72MHz RCC_PLLCmd(ENABLE); // wait until the PLL is ready while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET); // 4. Set system clock dividers RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5); RCC_ADCCLKConfig(RCC_PCLK2_Div8); RCC_PCLK2Config(RCC_HCLK_Div1); RCC_PCLK1Config(RCC_HCLK_Div2); RCC_HCLKConfig(RCC_SYSCLK_Div1); #ifdef EMB_FLASH // 5. Init Embedded Flash // Zero wait state, if 0 < HCLK 24 MHz // One wait state, if 24 MHz < HCLK 56 MHz // Two wait states, if 56 MHz < HCLK 72 MHz // Flash wait state FLASH_SetLatency(FLASH_Latency_2); // Half cycle access FLASH_HalfCycleAccessCmd(FLASH_HalfCycleAccess_Disable); // Prefetch buffer FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); #endif // EMB_FLASH // 5. Clock system from PLL RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); }////////////////////////////////
// // // //Start MAIN function // // // //////////////////////////////void main(void)
{ GPIO_InitTypeDef GPIO_InitStructure; #ifdef DEBUG debug(); #endif // Init clock system Clk_Init(); // GPIO Init // Enable GPIO clock and release reset RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOE, ENABLE); RCC_APB2PeriphResetCmd(RCC_APB2Periph_GPIOE, DISABLE); // Assign PE6 to LED GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
GPIO_Init(GPIOE, &GPIO_InitStructure); GPIO_WriteBit(GPIOE,GPIO_Pin_6,Bit_SET); while(1) { } }#ifdef DEBUG
/******************************************************************************* * Function Name : assert_failed * Description : Reports the name of the source file and the source line number * where the assert_param error has occurred. * Input : - file: pointer to the source file name * - line: assert_param error line source number * Output : None * Return : None *******************************************************************************/ void assert_failed(u8* file, u32 line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) *//* Infinite loop */
while (1) { } } #endif2011-09-16 7:40 AM
I have never had to initialize the HSI if using the HSE. But PLLCLK is connected to HSE, so that is probably not your problem.
I have never had to release the APB2 peripheral reset. Try commenting that line out. You don't identify the processor, so we have to assume PE6 is available. Single step through the code to make sure it executes as expected, and put a meter or scope on PE6 to make sure the problem is not a bad LED. Cheers, Hal2011-09-16 10:47 AM
If PE.6 doesn't work, try some other pins.
Stick a scope of the pin, and toggle it, lot more effective at identifying that we're talking about the right pin. Perhaps the LED is active LOW? The board should implicitly be running from the HSI to start with, if it's functional enough to be running code, you can set up the GPIO side of things with very little additional effort. For a peripheral reset to be helpful you need to ENABLE then DISABLE, so you actually get a reset pulse regardless of initial conditions, and it really needs a running synchronous clock first.void main(void)
{ GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOE, ENABLE); GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_Init(GPIOE, &GPIO_InitStructure); GPIO_SetBits(GPIOE,GPIO_Pin_6); while(1) { } }2011-09-16 12:08 PM
2011-09-16 12:21 PM
2011-09-16 12:27 PM
HELP! SIMPLE APP WONT WORK
THE LED IS ACTIVE LOW - YOU NEED TO DRIVE IT WITH ZERO TO ILLUMINATE IT. http://www.ebay.com/itm/ARM-Cortex-M3-STM32F103VET6-Mini-Development-Board-/190550067511?pt=LH_DefaultDomain_0&hash=item2c5dab4937 http://www.sendspace.com/file/6sh37k http://fs02n2.sendspace.com/dl/ae0a2c0b6991b8fc1db6f1fa4a2ed554/4e73a1d56d97b874/6sh37k/STM32F103VET6.pdf Note how the other end of the PE5/6 LED is connected to 3.3V VCC2011-09-16 1:38 PM
clive1 forgive my ignorance, u mean somethin like
GPIO_WriteBit(GPIOE,GPIO_Pin_6,Bit_RESET)? i tried this but still nothin.2011-09-16 6:21 PM
So what code line executed to trigger this fault? To answer that, you need to single step through the code. Cheers, Hal
2011-09-16 7:30 PM
2011-09-17 4:08 AM
Okay well, i cant get the fault to occur again but i think i found where the problem is starting.
at the very last instruction of the clock init function, the program dead ends at a mov instruction that goes no where. what could be causing this?