Hello,
I'm new on STM32. I'm using STM32F769-Discovery for product prototiping and I am trying to use USART6 with interrupts. That's what I've:
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-20 2:21 AM
#define UART_PORTID USART6//USART1
#define USARTx_CLK_ENABLE() __HAL_RCC_USART6_CLK_ENABLE();
#define USARTx_RX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOC_CLK_ENABLE()
#define USARTx_TX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOC_CLK_ENABLE()
#define USARTx_FORCE_RESET() __HAL_RCC_USART6_FORCE_RESET()
#define USARTx_RELEASE_RESET() __HAL_RCC_USART6_RELEASE_RESET()
#define USARTx_TX_PIN GPIO_PIN_6
#define USARTx_TX_GPIO_PORT GPIOC
#define USARTx_TX_AF GPIO_AF8_USART6
#define USARTx_RX_PIN GPIO_PIN_7
#define USARTx_RX_GPIO_PORT GPIOC
#define USARTx_RX_AF GPIO_AF8_USART6
UART_HandleTypeDef UART_Handle;
void USART6_IRQHandler()
{
HAL_UART_IRQHandler(&UART_Handle);
}
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO TX/RX clock */
USARTx_TX_GPIO_CLK_ENABLE();
USARTx_RX_GPIO_CLK_ENABLE();
/* Enable USART clock */
USARTx_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* UART TX GPIO pin configuration */
GPIO_InitStruct.Pin = USARTx_TX_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Alternate = USARTx_TX_AF;
HAL_GPIO_Init(USARTx_TX_GPIO_PORT, &GPIO_InitStruct);
/* UART RX GPIO pin configuration */
GPIO_InitStruct.Pin = USARTx_RX_PIN;
GPIO_InitStruct.Alternate = USARTx_RX_AF;
HAL_GPIO_Init(USARTx_RX_GPIO_PORT, &GPIO_InitStruct);
UART_Handle.Instance = UART_PORTID;
UART_Handle.Init.BaudRate = 9600;
UART_Handle.Init.WordLength = UART_WORDLENGTH_8B;
UART_Handle.Init.StopBits = UART_STOPBITS_1;
UART_Handle.Init.Parity = UART_PARITY_NONE;
UART_Handle.Init.Mode = UART_MODE_TX_RX;
UART_Handle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UART_Handle.Init.OverSampling = UART_OVERSAMPLING_16;
// Init USART
HAL_UART_Init( &UART_Handle);
// Enable USART IRQn
NVIC_EnableIRQ(USART6_IRQn);
void EwBspConsolePutCharacter( const char* aMessage, unsigned int size ){
HAL_UART_Transmit_IT( &UART_Handle, (uint8_t*)aMessage,(uint16_t)size);
}
And EwBspConsolePutCharacter is called from:
void EwConsoleOutput( const char* aMessage)
{
char buffer[] = "HelloWorld\n\r";
EwBspConsolePutCharacter(&buffer,sizeof(buffer));
}
The PC that receives the messages has serial config: 9600,8bits,1stopbit, non parity, none hw flowcontrol
The issue is sometimes message arrives incomplete:
Where could be the mistake?
Kind Regards,
Rafa
Solved! Go to Solution.
Labels:
- Labels:
-
STM32F7 Series
-
UART-USART
1 ACCEPTED SOLUTION
Accepted Solutions
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-20 8:55 AM
FIXED:
HAL_UART_Transmit_IT stores a pointer and length of the data buffer you provide. It doesn't perform a copy, so your buffer you passed needs to remain valid until callback gets called. For example it cannot be a buffer you'll perform delete [] / free on before callbacks happen or a buffer that's local in a function you're going to return from before a callback call.
So I have modified EwBspConsolePutCharacter to:
void EwBspConsolePutCharacter(char* aFrame,unsigned int aSize){
static char buffer[256];
// Assign to buffer the frame to be sent
for(unsigned int i = 0; i<aSize;i++){
buffer[i] = *(aFrame+i);
}
HAL_UART_Transmit_IT( &UART_Handle, (uint8_t*)&buffer,(uint16_t)aSize);
}
Now it's working as expected
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-20 8:55 AM
FIXED:
HAL_UART_Transmit_IT stores a pointer and length of the data buffer you provide. It doesn't perform a copy, so your buffer you passed needs to remain valid until callback gets called. For example it cannot be a buffer you'll perform delete [] / free on before callbacks happen or a buffer that's local in a function you're going to return from before a callback call.
So I have modified EwBspConsolePutCharacter to:
void EwBspConsolePutCharacter(char* aFrame,unsigned int aSize){
static char buffer[256];
// Assign to buffer the frame to be sent
for(unsigned int i = 0; i<aSize;i++){
buffer[i] = *(aFrame+i);
}
HAL_UART_Transmit_IT( &UART_Handle, (uint8_t*)&buffer,(uint16_t)aSize);
}
Now it's working as expected