cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I have a short circuit between the RESET and the VCC. I measure a impedance of 1ohm between these two signals and 80ohm with the GND. The RESET pin only goes on a 0.1UF capacitor and on the programming connector.

ludovic-micou2
Associate III

the ST-LINK can't detect the micro but the software who is already programmed in the micro work perfectly.

Does anyone have an explanation why the reset breaks like this?

2 REPLIES 2
TDK
Guru

If NRST is shorted to VCC, there's a hardware error or you've damaged the chip. There's no setting you can enable that would do this.

Likewise, if VCC has 80 Ohm impedance to ground, that also indicates a likely hardware error.

Also possible you're measuring it incorrectly, such as with the debugger attached or with it powered.

If you feel a post has answered your question, please click "Accept as Solution".
lmico.1
Associate

The measurement was made with the power and probe cables disconnected from the board. The measurement