2022-01-13 6:55 AM
the ST-LINK can't detect the micro but the software who is already programmed in the micro work perfectly.
Does anyone have an explanation why the reset breaks like this?
2022-01-13 7:12 AM
If NRST is shorted to VCC, there's a hardware error or you've damaged the chip. There's no setting you can enable that would do this.
Likewise, if VCC has 80 Ohm impedance to ground, that also indicates a likely hardware error.
Also possible you're measuring it incorrectly, such as with the debugger attached or with it powered.
2022-01-13 7:16 AM
The measurement was made with the power and probe cables disconnected from the board. The measurement