cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am working with STM32 Nucleo board (NUCLOE-H743ZI2),I have an issue while writing with external debugger stlinkV2. I have connected to microcontroller and able to read the flash memory but I was unable or erase or write into the memory.

GHARI.1
Associate II

0693W00000Kb3ycQAB.png0693W00000Kb40TQAR.png0693W00000Kb40iQAB.pngI am also attaching the error file from STLINK utility. Can anyone help to sort this thing out.

5 REPLIES 5
TDK
Guru

ST-Link Utility is NRND status. Does it work with STM32CubeProgrammer?

If you feel a post has answered your question, please click "Accept as Solution".

We are facing same issue with STM32CubeProgrammer.

We are getting write protection error and core halted errors so how to solve this issue.

Hello,

When you use the ST-LinkV2 embedded on the board, what do you get?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
MM..1
Chief III

As first why you dont do , what is in red on image. Change mode from Hotplug ....