cancel
Showing results for 
Search instead for 
Did you mean: 

Hello! I am working on a project using the STM32H747 dualcore. The M4 core is responsible among other tasks for sampling a fairly quick digital signal (5-10 Mhz). I am looking for a hardware interface on the H7 that will allow me to sample this signal.

yuri CH
Senior

the sampling logic and countig is not very standard:

1)     If A = rising edge and B = 0, counter++

2)     If A = falling edge and B = 1, counter++

3)     If B = rising edge and A = 1, counter++

4)     If B = falling edge and A = 0, counter++

5)     If A = falling edge and B = 0, counter--

6)     If A = rising edge and B = 1, counter--

7)     If B = rising edge and A = 0, counter--

8)     If B = falling edge and A = 1, counter-- 

Since the M4 core is doing other things during the sampling i do not want to use interrupts as the solution to this problem.

Please help me understand wether this is possible using some king of HW interface (perhaps timer?)

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0