Hello everyone.
I'm using a ADC with DMA.
The device is stm32l073.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-09 9:09 PM
If the ADC is used alone without using DMA, the data conversion will be performed in the cycle described in the data sheet.
However, the conversion time is doubled when using DMA.
Do you know why?
Common conditions
・Clock : 16MHz
・Clock Prescaler : Asynchronous clock mode divided by 1
・Resolution : 12bit
・Continuous Conversion Mode : Enabled
・Overrun behaviour : overwritten
・Oversampling Mode Enabled
・Sampling ratio : 64
・Triggered Mode : Single trigger
・Sampling time : 1.5
・External Trigger Conversion Source : Regular conversion
Different conditions
・DMA Continuous Requests : Enabled / Disabled
regard.
- Labels:
-
ADC
-
DMA
-
Interrupt
-
STM32L0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-10 11:40 PM
Is DMA and oversampling incompatible?