2015-06-05 12:16 PM
I am a Stm32 new learner.Recently I have had two Stm32 chips to communicated with eachother by using it wardware SPI.After I wrote the master and slave program and downloaded it into both stm32 chips.I used a logic analytical device to observe the wave of MOSI,MISO and clock.I found that the wave(the master date) from the Master was correct,but the data the master received from the slave was wrong.For example I want to send 0xff to the slave and the slave feedback 0x32 to the master(I can see 11111111 coming out from the MOSI,but from the MISO I saw 11001000 not 00110010).I don't know why,I checked both of my program,the polarity are the same and the mode setting is right.
here is my master programint main(void){ SPI_InitTypeDef SPI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; ErrorStatus HSEStartUpStatus; RCC_DeInit(); //ÅäÖÃRCCʱÖÓ// RCC_HSEConfig(RCC_HSE_ON); HSEStartUpStatus = RCC_WaitForHSEStartUp(); if(HSEStartUpStatus == SUCCESS) { RCC_HCLKConfig(RCC_SYSCLK_Div1); RCC_PCLK2Config(RCC_HCLK_Div1); RCC_PCLK1Config(RCC_HCLK_Div2); FLASH_SetLatency(FLASH_Latency_2); FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9); RCC_PLLCmd(ENABLE); while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { } } RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA, ENABLE ); //³õʼ»¯GPIO¡¡// GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_SetBits(GPIOA,GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE ); //³õʼ»¯SPI SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI1, &SPI_InitStructure); SPI_Cmd(SPI1, ENABLE); SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE); SPI1_ReadWriteByte(0xff); while(1); }the slave programint main(void){ SPI_InitTypeDef SPI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; ErrorStatus HSEStartUpStatus; RCC_DeInit(); //ÅäÖÃRCCʱÖÓ// RCC_HSEConfig(RCC_HSE_ON); HSEStartUpStatus = RCC_WaitForHSEStartUp(); if(HSEStartUpStatus == SUCCESS) { RCC_HCLKConfig(RCC_SYSCLK_Div1); RCC_PCLK2Config(RCC_HCLK_Div1); RCC_PCLK1Config(RCC_HCLK_Div2); FLASH_SetLatency(FLASH_Latency_2); FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9); RCC_PLLCmd(ENABLE); while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { } } RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA, ENABLE ); //³õʼ»¯GPIO¡¡// GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_SetBits(GPIOA,GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE ); //³õʼ»¯SPI SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Slave; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI1, &SPI_InitStructure); SPI_Cmd(SPI1, ENABLE); SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE); SPI1->DR=0x32; while(1); }I want to explain why I only writeSPI1->DR=0x32 in slave program.cos I readed some documents about SPI,It tells me that SPI slave will communicate with the master automatically as the clock signal coming from the master.I just want them exchange one byte data,So I gave one date to SPI->DR directively.What's wrong with my program or did I get the SPI process wrong???I am curious if SPI->DR=0xdata works,it can be worng,and I see the sample of ST,they also use
SPI->DR=0xdata,but now I got a wrong MISO wave....why???
I sincerely want to get some help from you.Thank you very much best regards2015-06-05 12:53 PM
You probably shouldn't enable interrupts unless you have code to configure and handle them.
You should pay attention to the state of the status register *before* randomly outputting data. Consider if you need to be looking for a chip-select, and how you expect the two STM32 to be synchronized before you start sending data. ie at the very least wait until the slave signals that it's ready before sending data to it.Are you using CooCox? Shouldn't the SPL/CMSIS SystemInit() code get the PLL running?2015-06-07 2:51 AM
2015-06-07 4:29 AM
And I also readed some article saying that when Stm32 act as the slave, its baud rate should be lower than the master.But I couldn't understand.In my opinion,the baud rate of the slave has nothing to do with the SPI process.because spi commucation is under the control of the master clock,so once I configurate the master,the slave have nothing to do but receiving datas from the master whild giving datas back to the master based on the master speed.Could u tell me if what that article mentioned is wrong?Thank you very much
2015-06-09 5:34 AM
The management of the GPIO and SPI interfaces in not the same for al members of the STM32 family.
If you are using a STM32F1XX MCU pin PA5 (SCK) and PA7(MOSI) of the slave and pin PA6 (MISO) of the master should be initialized in INPUT MODE and not as Alternate Function PP.B.R.Danilo