2020-12-02 2:19 PM
The ram on the STM32H7 is segmented into non-contiguous sections. How would one be able to dynamically allocate memory in different sections of RAM? eg: put large objects in AXI-SRAM and small object that need fast access on DTCM.
I'm wondering if this is possible without a custom allocator however, links to open-source custom allocators or ideas for writing simple allocator would be appreciated.
2020-12-02 2:49 PM
2020-12-02 3:45 PM
My lazy approach in Keil was to stuff the additional regions into the the allocators linked-list.
Realistically you probably need different pools
2020-12-02 4:25 PM
Interesting, I also think that different pools are necessary since I would like to explicitly select the pool with which I am working. The "LwMEM" library mentioned by @Piranha has the features I'm looking for. Not sure about the reliability since it is under active development. It does have a few unit tests and decent documentation so that is a good start.
2020-12-03 10:16 AM
These lost something in the forum transition, and I can't edit them, but for completeness, and so I don't have to search again
https://community.st.com/s/question/0D50X00009XkgWSSAZ/locate-heap-in-sdram
2021-05-11 7:33 AM
Code on master branch or under releases is usually passing the tests. Of course it doesn't mean it is bug free :)
I welcome you to contribute if you believe you need more features.