2022-04-12 2:15 AM
Hi,
I'm working on SDMMC on STM32U5 nucleo board.
Everything works fine for 1 and 4 bit mode.
But, in 8 bit mode I can write data with HAL_MMC_WriteBlocks but when I try to read back with HAL_MMC_ReadBlocks, it always gets SDMMC_FLAG_DCRCFAIL.
Have you ever met the same error? If yes, how did you solve it.
Thanks in advance
2022-05-14 12:27 AM
I have met this same error SDMMC_FLAG_DCRCFAIL with HAL_SD_ReadBlocks. Using 4-bit wide data bus.
Do you have advice?