cancel
Showing results for 
Search instead for 
Did you mean: 

Hard to track down the actual cause.

Posted on November 09, 2016 at 06:13

Hi,

In the project properties setting, I am using arm-none-eabi-gcc toolchain.

This time toolchain is Ac6 STM32 MCU GCC and builder CDT internal.

Problem is if I add h files in HAL library that error log suggest me to do, it solved and if I build project again it shows the problem in CMSIS include H files.

0690X0000060MnYQAU.gif

Such as,

1. C:\STM32_toolchain\common\Drivers\CMSIS\Device\ST\STM32F0xx\Include/stm32f0xx.h:187:3: error: declaration for parameter 'FunctionalState' but no such parameter

} FunctionalState;

^

..\inc\Src\stm32f0xx_hal_flash_ex.c:990:1: error: expected '{' at end of input

}

^

..\inc\Src\stm32f0xx_hal_flash_ex.c:990:1: warning: control reaches end of non-void function [-Wreturn-type]

}

^

APIs, Headers,state machine files are exists in Project branch, but why the compiler showing errors in H files of driver ?

Looking at C code structure related reason, yes I found some style of C coding in CMSIS h files is different.

what should I do now?

1. CDT does not showing errors of my main files, there was a return type problem, I solved it.

3. I think compiler is compiling all files listed in project branch , do you want me to remove some of the files from project folder, is it repeating again as I include paths from C driver?

4. Is there any setting for which only compile my c file?

5. Do you believe, updated version of Java/gcc/Eclipse is needed ?

I am using this HAL driver STM32Cube_FW_F0_V1.6.0 downloaded from STM website.

Hope you will give me some good suggestions.

Regards

HASAN

#arm-cmsis-driver-pack #error #error #demonstration-builder #adding-files-to-the-project #arm-gcc #know-your-tools #arm-gcc #gcc

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This discussion is locked. Please start a new topic to ask your question.
46 REPLIES 46
Posted on December 14, 2016 at 07:10

Hello Mr Kraal,

Thank you for your suggestion.

I will be keep doing things you explains.

Did you mean I should do it for clearing build confusion? Or project settings in Eclipse ?

Besides this stm provided, TM32Cube_FW_F0_V1.6.0.

As far as I remembered  I have opened those project, build successfully.

Here we mainly discussed about custom project build errors.

Regards

Hasan

Posted on December 14, 2016 at 09:30

Hello Mr. Hasan,

I understood that the thread was about build errors for custom project. In the link I provided, the author goes from scratch to build a custom project (the classic blinky), and you can see all the errors he encounters all along the process.

I used this link to get up and running with a clean eclipse setup, and to be able to make any custom project I want on any F0, F3 or F4 (I'm using the SPL as I don't like Cube at all, and I'm leaning towards direct register access as I used to do on AVR).

Also you seemed to have tried many different IDEs without success. So maybe you should concentrate on 1 IDE and get it running, otherwise you waste your time trying everything for all different IDEs.

Regards,

Carl

Posted on December 14, 2016 at 09:42

Thank you to help me. 

Right at the moment, 'getting started '  has not finished for me I know.

I got little understanding about , include paths, pre-processor  reasons, there are thousands of setting is in Ecilipse I know.

Link you provided is helpful for sure.

I'm using the SPL as I don't like Cube at all,

Give me some reference and institutions. 

Posted on December 14, 2016 at 14:04

SPL stands for Standard Peripherals Library. You can get the F0 version there : 

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libraries/stsw-stm32048.html

.

Once unzipped, look for the .chm file which provides a few hints on how to use it (the chapter 'How to use the Standard Peripherals Library').

The rest is up to you.

Posted on December 16, 2016 at 05:41

Mr, Kraal,

Thank you or this tools.

Have you ever use Cubemx?

If you did so, what difference you feel among two?

Posted on December 16, 2016 at 09:17

No I'm sorry but I have never used CubeMX, so I can't comment on this.

Posted on December 16, 2016 at 10:07

Ok, then suggest me any example project can open in SPL

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fembedded-software%2Fmcus-embedded-software%2Fstm32-embedded-software%2Fstm32-standard-peripheral-libraries%2Fstsw-stm32html

.