HAL SAI cannot run quick enough for basic audio sampling?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-05-24 6:16 AM
I am trying to take a microphone sample every 62.5 microseconds (16,000Hz) which is the standard rate for audio files.
The problem i have found is that HAL_SAI_Receive_DMA() returns HAL_BUSY for some samples. So we dont receive the required 16,000 samples in the 1 second, it only manages 14750.
The SAI component can reach rates of 192KHz so it makes no sense that it cannot handle 16KHz? So how do i fix the problem of receiving HAL_BUSY?
Thanks!
Here is an example sketch running on an STML452RE:
#include <SoftwareSerial.h>
#include <Arduino.h>
#include <HardwareTimer.h>
#include "stm32l4xx.h"
#include "stm32l4xx_hal.h"
#include "stm32l4xx_hal_def.h"
#include "stm32l4xx_hal_gpio.h"
#include "stm32l4xx_hal_sai.h"
#include "stm32l4xx_hal_exti.h"
#include "stm32l4xx_hal_cortex.h"
#include "Sysclock_Config.h"
GPIO_InitTypeDef gpioInit;
SAI_HandleTypeDef saiHandle;
RCC_PeriphCLKInitTypeDef periphInit;
DMA_HandleTypeDef hdmaInit;
uint8_t SAIDataBuffer[8] = { 0 };
HardwareTimer hardwareTimer(TIM3);
void assert_failed(uint8_t* inFileName, uint32_t line)
{
char* fileNameAsString = (char*)inFileName;
Serial2.println(F("*** [HAL ASSERT FAILED] ***"));
Serial2.printf("%s\r\n", (char*)inFileName);
Serial2.printf("%i\r\n", line);
}
void _Error_Handler(const char* file, int line)
{
Serial2.println(F("*** [ERROR HANDLED] ***"));
Serial2.printf("%s\r\n", file);
Serial2.printf("%i\r\n", line);
}
extern "C"
{
void HAL_SAI_TxHalfCpltCallback(SAI_HandleTypeDef* hsai)
{
}
void HAL_SAI_TxCpltCallback(SAI_HandleTypeDef* hsai)
{
}
void HAL_SAI_RxHalfCpltCallback(SAI_HandleTypeDef* hsai)
{
}
void HAL_SAI_RxCpltCallback(SAI_HandleTypeDef* hsai)
{
}
void HAL_SAI_ErrorCallback(SAI_HandleTypeDef* hsai)
{
}
__weak void SAI1_IRQHandler(void)
{
HAL_SAI_IRQHandler(&saiHandle);
}
__weak void DMA2_Channel1_IRQHandler(void)
{
/* USER CODE BEGIN DMA2_Channel1_IRQn 0 */
/* USER CODE END DMA2_Channel1_IRQn 0 */
HAL_DMA_IRQHandler(&hdmaInit);
/* USER CODE BEGIN DMA2_Channel1_IRQn 1 */
/* USER CODE END DMA2_Channel1_IRQn 1 */
}
}
void samplerCallback();
// the setup function runs once when you press reset or power the board
void setup()
{
delay(5000);
Serial2.begin(115200);
Serial2.println("Starting");
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_DMA2_CLK_ENABLE();
__HAL_RCC_SAI1_CLK_ENABLE();
gpioInit.Pin = GPIO_PIN_15 | GPIO_PIN_10 | GPIO_PIN_12;
gpioInit.Mode = GPIO_MODE_AF_PP;
gpioInit.Pull = GPIO_NOPULL;
gpioInit.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
gpioInit.Alternate = GPIO_AF13_SAI1;
HAL_GPIO_Init(GPIOB, &gpioInit);
pinMode(PB1, OUTPUT);
digitalWrite(PB1, LOW);
saiHandle.Instance = SAI1_Block_A; // audio block A.
saiHandle.Init.Protocol = SAI_FREE_PROTOCOL;
saiHandle.Init.FirstBit = SAI_FIRSTBIT_MSB;
saiHandle.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_16K;
saiHandle.Init.AudioMode = SAI_MODEMASTER_RX; // block a must provide clock signals and receive from the data line.
saiHandle.Init.Synchro = SAI_ASYNCHRONOUS; // we only want to use this one audio block.
saiHandle.Init.SynchroExt = SAI_SYNCEXT_DISABLE; // disable sychronizing the 2 audio blocks.
saiHandle.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE; // assume to power the data?
saiHandle.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE; // any frame length allowed.
saiHandle.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY; // used for interrupts.
saiHandle.Init.MonoStereoMode = SAI_STEREOMODE; // mono mode only available in transmission mode.
saiHandle.Init.CompandingMode = SAI_NOCOMPANDING; // telecommunications specification (not needed)
saiHandle.Init.TriState = SAI_OUTPUT_NOTRELEASED; // assume the SAI is ma
saiHandle.FrameInit.FrameLength = 64; // 64 bit frame. (2 slots)
saiHandle.FrameInit.ActiveFrameLength = 32; // Frame synchronization active level length. (half the frame length)
saiHandle.FrameInit.FSDefinition = SAI_FS_CHANNEL_IDENTIFICATION;
saiHandle.FrameInit.FSPolarity = SAI_FS_ACTIVE_LOW;
saiHandle.FrameInit.FSOffset = SAI_FS_BEFOREFIRSTBIT;
saiHandle.SlotInit.FirstBitOffset = 0; // no offset in receive mode -> FBOFF <= (SLOTSZ - DS)
saiHandle.SlotInit.SlotSize = SAI_SLOTSIZE_32B; // 32 bits per slot to contain the 32 data bits (24 data, 8 zeroed)
saiHandle.SlotInit.SlotNumber = 2;
saiHandle.SlotInit.SlotActive = SAI_SLOTACTIVE_ALL;
hdmaInit.Instance = DMA2_Channel1;
hdmaInit.Init.Request = DMA_REQUEST_1;
hdmaInit.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdmaInit.Init.PeriphInc = DMA_PINC_DISABLE;
hdmaInit.Init.MemInc = DMA_MINC_ENABLE;
hdmaInit.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdmaInit.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdmaInit.Init.Mode = DMA_NORMAL;
hdmaInit.Init.Priority = DMA_PRIORITY_VERY_HIGH;
if (HAL_DMA_Init(&hdmaInit) != HAL_OK)
{
Error_Handler();
}
/* Several peripheral DMA handle pointers point to the same DMA handle.
Be aware that there is only one channel to perform all the requested DMAs. */
__HAL_LINKDMA(&saiHandle, hdmarx, hdmaInit);
__HAL_LINKDMA(&saiHandle, hdmatx, hdmaInit);
HAL_NVIC_SetPriority(DMA2_Channel1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA2_Channel1_IRQn);
HAL_NVIC_SetPriority(SAI1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SAI1_IRQn);
HAL_StatusTypeDef saiStatus = HAL_SAI_InitProtocol(&saiHandle,
SAI_I2S_STANDARD, // runs the SAI_InitI2S() function.
SAI_PROTOCOL_DATASIZE_24BIT,// 24 bits (24 bit is standard for I2S).
2); // number of slots per frame - 1
__HAL_SAI_ENABLE(&saiHandle);
if (saiStatus != HAL_OK)
{
Serial2.println("SAI ERROR");
while (1) {}
}
else
{
Serial2.println("Sai init ok.");
}
hardwareTimer.setMode(1, TIMER_OUTPUT_COMPARE, NC); // remove this for new version of STM32Dino, required version 1.8.0.
hardwareTimer.setOverflow(16000, HERTZ_FORMAT);
hardwareTimer.detachInterrupt();
hardwareTimer.attachInterrupt(samplerCallback);
hardwareTimer.resume();
Serial2.flush();
start = millis();
}
int32_t GetSample()
{
uint8_t a1 = SAIDataBuffer[0];
uint8_t b1 = SAIDataBuffer[1];
uint8_t c1 = SAIDataBuffer[2];
uint8_t d1 = SAIDataBuffer[3];
uint8_t a2 = SAIDataBuffer[4];
uint8_t b2 = SAIDataBuffer[5];
uint8_t c2 = SAIDataBuffer[6];
uint8_t d2 = SAIDataBuffer[7];
// value as signed 24 bit integer
int32_t slot24sb = 0;
slot24sb = slot24sb | (a1 << 8);
slot24sb = slot24sb | (b1 << 16);
slot24sb = slot24sb | (c1 << 24);
slot24sb = slot24sb >> 8;
return slot24sb;
}
int num_samples = 0;
void samplerCallback(void)
{
HAL_StatusTypeDef rxResponse;
rxResponse = HAL_SAI_Receive_DMA(&saiHandle, SAIDataBuffer, 2U);
int sample = GetSample();
if (rxResponse != HAL_OK)
{
//Serial2.println("Error in SAI");
}
else
{
num_samples++;
}
}
// the loop function runs over and over again until power down or reset
void loop()
{
if (millis() - start > 1000)
{
Serial2.println(num_samples);
while (1) {}
}
}
Solved! Go to Solution.
- Labels:
-
SAI
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-05-24 11:49 AM
The issue was that the Master Clock Divider was not configured correctly and that samples need to be handled in the "Transfer Complete" callback. Thank you @Community member and @Community member

- « Previous
-
- 1
- 2
- Next »