Skip to main content
Senior
January 28, 2021
Solved

HAL_QSPI_AutoPolling() fail when polling the SR of NOR flash in QPI mode

Hi,

I'm using STM32H750B with a NOR flash (Winbond's W25128 chip). When the chip is configured as QPI mode. If polling SR1 using the auto polling function, it will throw error. But read SR directly and check the bits works.

Any help? Thanks.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
February 10, 2021

I confirm that W25Q128JV-DTR supports QPI mode.

Can you try your indirect mode configuration (4-4-4) and add 1 or 2 Dummy-cycles ? for example: qspi_cmd->DummyCycles = 2;

Then, please keep me informed about your progress on this.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

11 replies

ST Technical Moderator
January 28, 2021

Hello @diverger​ ,

Please share your QUADSPI configuration to help you resolve your issue.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
divergerAuthor
Senior
January 30, 2021

The pseudo code is as below:

// Send ERASE_SECTOR_CMD

send(ERASE_SECTOR_CMD);

// Auto Polling

qspi_cmd->InstructionMode = QSPI_INSTRUCTION_4_LINES;

qspi_cmd->Instruction = 0x05;

qspi_cmd->AddressMode = QSPI_ADDRESS_NONE;

qspi_cmd->AddressSize = QSPI_ALTERNATE_BYTES_24_BITS;

qspi_cmd->AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;

qspi_cmd->AlternateBytes = 0;

qspi_cmd->AlternateBytesSize = 0;

qspi_cmd->DummyCycles = 0;

qspi_cmd->DataMode = QSPI_DATA_4_LINES;

qspi_cmd->DdrMode = QSPI_DDR_MODE_DISABLE;

qspi_cmd->DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;

qspi_cmd->SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

qspi_cmd->Address = 0;

qspi_cmd->NbData = 0;

qspi_poll->Match = 0x00;

qspi_poll->Mask = 0x01;

qspi_poll->MatchMode = QSPI_MATCH_MODE_AND;

qspi_poll->StatusBytesSize = 1;

qspi_poll->Interval = 0x16;

qspi_poll->AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;

HAL_QSPI_AutoPolling(qspi_hdl, qspi_cmd, qspi_poll, timeout_ms);

Thanks.

ST Technical Moderator
February 4, 2021

Hi @diverger​ ,

I see you are trying to use QUAD 4-4-4 mode, memories that support this mode require to enable it.

Are you sure that the memory support the Quad mode ? If yes, did you correctly enable it ? Please share the exact memory part number.

Can you please test the following configuration:

qspi_cmd->InstructionMode = QSPI_INSTRUCTION_1_LINE;
qspi_cmd->Instruction = 0x05;
qspi_cmd->AddressMode = QSPI_ADDRESS_NONE;
qspi_cmd->AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
qspi_cmd->DummyCycles = 0;
qspi_cmd->DataMode = QSPI_DATA_1_LINE;
qspi_cmd->DdrMode = QSPI_DDR_MODE_DISABLE;
qspi_cmd->DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
qspi_cmd->SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
 
qspi_poll->Match = 0x00;
qspi_poll->Mask = 0x01;
qspi_poll->MatchMode = QSPI_MATCH_MODE_AND;
qspi_poll->StatusBytesSize = 1;
qspi_poll->Interval = 0x10;
qspi_poll->AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;
 
HAL_QSPI_AutoPolling(qspi_hdl, qspi_cmd, qspi_poll, timeout_ms);

Then, please keep me informed about your progress on this issue.

I also advise you to have a look at this AN4760: Quad-SPI interface on STM32 microcontrollers and microprocessors, this will help you on the Quad-SPI interface and configuration.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
divergerAuthor
Senior
February 5, 2021

Yes, I'm sure I've enabled the QPI mode. And I can use normal read and check (in QPI mode) the status, and it works well. But it seems the auto-polling function won't work in this mode. My chip is w25q128jv.

ST Technical Moderator
February 8, 2021

Hi @diverger​ ,

I found different info that you may want to check: according to the W25Q128JV datasheet, the read status register is only in standard SPI mode (1-1-1).

0693W000007EI9RQAW.jpg 

For more details, please check the W25Q128JV datahseet , in sections:

  • 8.1.2 Instruction Set Table 1 (Standard SPI Instructions)
  • 8.1.3 Instruction Set Table 2 (Dual/Quad SPI Instructions)
  • 8.2.4 Read Status Register-1 (05h), Status Register-2 (35h) & Status Register-3 (15h)

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
divergerAuthor
Senior
February 10, 2021

Hi @Imen DAHMEN​ Thanks for your patience.

Actually I'm not very sure if my chip is W25Q128JV or W25Q128JV-DTR (the chip is on a EVAL-board, and I need ask for the BOM to get the exact part number), the latter one apparently supports this command in QPI mode. And I can read the JESD SFDP table, it shows it support DTR, so my chip is very likely the latter one. And another evidence is, I can read back the status register in QPI mode (using 4-4-4 line pattern) indeed. As you know, auto-polling is just making the read-and-check more 'auto', they use same command.

Thanks.

Imen.DBest answer
ST Technical Moderator
February 10, 2021

I confirm that W25Q128JV-DTR supports QPI mode.

Can you try your indirect mode configuration (4-4-4) and add 1 or 2 Dummy-cycles ? for example: qspi_cmd->DummyCycles = 2;

Then, please keep me informed about your progress on this.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
divergerAuthor
Senior
February 12, 2021

Hi, @Imen DAHMEN​ 

I tried two cases:

  1. As you have recommended, adding 2 dummy waiting clocks will work. Both 0 and 1 waiting clocks won't work.
  2. After sending the erase command, wait some time, then auto polling the SR will work too.

Any conclusion? Are there some reasons related with timing or clock frequency?

Thanks.

ST Technical Moderator
February 12, 2021

Hi @diverger​,

I'm glad to know that your issue is solved

In order to assure enough “turn-around�? time for changing the data signals from output mode to input mode, there must be at least one dummy cycle when using dual or quad mode to receive data from the Flash memory.

So, the QSPI require to insert two dummy-cycle in order to read correctly in quad mode, and this will not impact the read transfer from the status register.

The memory will always output the status register since it's clocked.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
divergerAuthor
Senior
February 12, 2021

Hi @Imen DAHMEN​ ,

I'm a little confused.

  1. The 'dummy' cycles will be insert between the instruction and the data phase (no address phase), right?
  2. Why normal read-check method work *only* without dummy clocks?
  3. In the DTR datasheet section 8.2.4, it doesn't show instruction 05h need extra dummy cycles in QPI mode, so, is this a undocumented trick?
  4. It seems, in QPI mode + auto-polling, the dummy clocks can be larger than 2, such as 4, 10, etc., will work too.

Thanks.

ST Technical Moderator
February 15, 2021

Hi @diverger​ ,

When reading with QUADSPI interface in Dual or Quad mode, you should insert at least one dummy cycle, in order to give output signals enought time to switch from output mode to input mode.

You can find this mentionned in Reference Manual section 23.3.3 QUADSPI command sequence "Dummy-cycles phase". This concern any command in Dual or Quad mode.

Even if it worked in indirect mode, for proper usage, you must follow the recommended QUADSPI specification to insert at least a dummy cycle.

In your case you are reading from a memory's status register the memory will always send its status register as long as it is clocked. So inserting dummy cycles will not impact the data transfert.

The QUADSPI will ignore the first status byte sent by the memory (2 dummy cycles) and will read the second one.

Hope it is clear and this brings some help to you.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks