2023-04-16 03:53 AM - edited 2023-11-20 08:04 AM
So I've created a project and am trying to use the HAL_delay(10); but it gets stuck at this function when im trying to debug.
I have been changing the clock and enabling the TIM2 so I don't know if i've messed something up. Here are the settings that I have:
And that is about it
2023-04-16 10:30 AM
I have that
2023-04-16 12:06 PM
int main(void)
{
/* USER CODE BEGIN 1 */
uint8_t buf[256];
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_SPI1_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_Base_Start(&htim2);
//HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x77<<1), 10, 100);
//HAL_Delay(500);
// read
// HAL_Delay(1000);
uint8_t koefS1_0 [2]={0}, koefS1_1 [2]={0},koefS1_2 [2]={0},koefS1_3 [2]={0},koefS1_4 [2]={0};
uint8_t koefS2_0 [2]={0}, koefS2_1 [2]={0},koefS2_2 [2]={0},koefS2_3 [2]={0},koefS2_4 [2]={0};
uint8_t koefI2C_0 [2]={0}, koefI2C_1 [2]={0},koefI2C_2 [2]={0},koefI2C_3 [2]={0},koefI2C_4 [2]={0};
uint8_t dataS1[3];
uint8_t dataS2[3];
uint8_t dataI2C[3];
dataS1[0] = 255,dataS1[1] = 255, dataS1[2] = 255;
dataS2[0] = 255,dataS2[1] = 255, dataS2[2] = 255;
dataI2C[0] = 255,dataI2C[1] = 255, dataI2C[2] = 255;
HAL_StatusTypeDef ret;
uint8_t command;
//SPI
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_SET);
//delay(1);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_RESET);
command = 0x1E;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(0x77<<1), &command, 1, 100);
// Enable write enable latch (allow write operations)
command = 0x48;
//delay(1);
HAL_SPI_Transmit(&hspi1, &command, 1, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_SET);
//READ SPI
command = 0x00;
//delay(1);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_RESET);
ret = HAL_SPI_Transmit(&hspi1,&command, 1, 100);
delay(1);
ret = HAL_SPI_Receive(&hspi1, dataS1, 3, 100);
//delay(1);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_SET);
command = 0xA2;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_RESET);
ret = HAL_SPI_Transmit(&hspi1,&command, 1, 100);
//delay(1);
ret = HAL_SPI_Receive(&hspi1, koefS1_4, 2, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_SET);
//delay(10);
command = 0xA4;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_RESET);
ret = HAL_SPI_Transmit(&hspi1,&command, 1, 100);
delay(1);
ret = HAL_SPI_Receive(&hspi1, koefS1_3, 2, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_SET);
//delay(10);
command = 0xA6;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_RESET);
ret = HAL_SPI_Transmit(&hspi1,&command, 1, 100);
//delay(10);
ret = HAL_SPI_Receive(&hspi1, koefS1_2, 2, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_SET);
//delay(10);
command = 0xA8;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_RESET);
ret = HAL_SPI_Transmit(&hspi1,&command, 1, 100);
delay(1);
ret = HAL_SPI_Receive(&hspi1, koefS1_1, 2, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_SET);
//delay(10);
__HAL_TIM_CLEAR_FLAG(&htim2, TIM_FLAG_UPDATE);
command = 0xAA;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_RESET);
ret = HAL_SPI_Transmit(&hspi1,&command, 1, 100);
delay(1);
//delay(1);
ret = HAL_SPI_Receive(&hspi1, koefS1_0, 2, 100);
//delay(1);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_SET);
uint32_t data_zdruzen = ((uint8_t)dataS1[0] << 16) | ((uint8_t)dataS1[1] << 8) | (uint8_t)dataS1[2];
uint16_t koef_zdruzen0 = ((int8_t)koefS1_0[0] << 8) | (koefS1_0[1]);
uint16_t koef_zdruzen1 = ((int8_t)koefS1_1[0] << 8) | (koefS1_1[1]);
uint16_t koef_zdruzen2 = ((int8_t)koefS1_2[0] << 8) | (koefS1_2[1]);
uint16_t koef_zdruzen3 = ((int8_t)koefS1_3[0] << 8) | (koefS1_3[1]);
uint16_t koef_zdruzen4 = ((int8_t)koefS1_4[0] << 8) | (koefS1_4[1]);
uint16_t data_zdruzen_16b = (uint16_t)(data_zdruzen>>8);
float temperatura1 = (-2)*koef_zdruzen4*pow(10,-21)*pow((float)data_zdruzen_16b,4)+ 4*koef_zdruzen3*pow(10,-16)*pow((float)data_zdruzen_16b,3)-2*koef_zdruzen2*pow(10,-11)*pow((float)data_zdruzen_16b,2)+1*koef_zdruzen1*pow(10,-6)*(float)data_zdruzen_16b+(-1.5)*koef_zdruzen0*pow(10,-2);
//long double temperatura = (-2)*koef_zdruzen4*pow(10,-21)*pow((double)data_zdruzen,4)+ 4*koef_zdruzen3*pow(10,-16)*pow((double)data_zdruzen,3)-2*koef_zdruzen2*pow(10,-11)*pow((double)data_zdruzen,2)+1*koef_zdruzen1*pow(10,-6)*(double)data_zdruzen+(-1.5)*koef_zdruzen0*pow(10,-2);
///////////////////////////////////////
#define ADDRESS (0x77)
#ifdef _TEST_
for(uint8_t i=1; i<256; i++)
{
ret = HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(i<<1), 10, 100);
if (ret != HAL_OK) /* No ACK Received At That Address */
{
//HAL_UART_Transmit(&huart1, Space, sizeof(Space), 10000);
}
else if(ret == HAL_OK)
{
//sprintf(buf, "0x%X", i);
//HAL_UART_Transmit(&huart1, buf, sizeof(buf), 10000);
}
buf[i] = (uint8_t)ret;
}
#endif
ret = HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(ADDRESS<<1), 10, 100);
//reset
command = 0x1E;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(ADDRESS<<1), &command, 1, 100);
// read
command = 0x48;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(ADDRESS<<1), &command, 1, 100);
//delay(1);
command = 0x00;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(ADDRESS<<1), &command, 1, 100);
//delay(1);
ret = HAL_I2C_Master_Receive (&hi2c1, (uint16_t)(ADDRESS<<1), dataI2C, 3, 100);
command = 0xA2;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(ADDRESS<<1), &command, 1, 100);
// delay(1);
ret = HAL_I2C_Master_Receive (&hi2c1, (uint16_t)(ADDRESS<<1), koefI2C_4, 2, 100);
command = 0xA4;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(ADDRESS<<1), &command, 1, 100);
//delay(1);
ret = HAL_I2C_Master_Receive (&hi2c1, (uint16_t)(ADDRESS<<1), koefI2C_3, 2, 100);
command = 0xA6;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(ADDRESS<<1), &command, 1, 100);
//delay(1);
ret = HAL_I2C_Master_Receive (&hi2c1, (uint16_t)(ADDRESS<<1), koefI2C_2, 2, 100);
command = 0xA8;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(ADDRESS<<1), &command, 1, 100);
//delay(1);
ret = HAL_I2C_Master_Receive (&hi2c1, (uint16_t)(ADDRESS<<1), koefI2C_1, 2, 100);
command = 0xAA;
ret = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t)(ADDRESS<<1), &command, 1, 100);
//delay(1);
ret = HAL_I2C_Master_Receive (&hi2c1, (uint16_t)(ADDRESS<<1), koefI2C_0, 2, 100);
//zdruzevanje podatkov
uint32_t data_zdruzenI2C = ((uint8_t)dataI2C[0] << 16) | ((uint8_t)dataI2C[1] << 8) | (uint8_t)dataI2C[2];
uint16_t koef_zdruzenI2C0 = ((int8_t)koefI2C_0[0] << 8) | (koefI2C_0[1]);
uint16_t koef_zdruzenI2C1 = ((int8_t)koefI2C_1[0] << 8) | (koefI2C_1[1]);
uint16_t koef_zdruzenI2C2 = ((int8_t)koefI2C_2[0] << 8) | (koefI2C_2[1]);
uint16_t koef_zdruzenI2C3 = ((int8_t)koefI2C_3[0] << 8) | (koefI2C_3[1]);
uint16_t koef_zdruzenI2C4 = ((int8_t)koefI2C_4[0] << 8) | (koefI2C_4[1]);
//temp
uint16_t data_zdruzenI2C_16b = (uint16_t)(data_zdruzenI2C>>8);
long double temperaturaI2C = (-2)*koef_zdruzenI2C4*pow(10,-21)*pow((double)data_zdruzenI2C_16b,4)+ 4*koef_zdruzenI2C3*pow(10,-16)*pow((double)data_zdruzenI2C_16b,3)-2*koef_zdruzenI2C2*pow(10,-11)*pow((double)data_zdruzenI2C_16b,2)+1*koef_zdruzenI2C1*pow(10,-6)*(double)data_zdruzenI2C_16b-1.5*koef_zdruzenI2C0*pow(10,-2);
This is my main function code. I have also found out that if I comment out SPI communication then I2C works but if I uncomment it and use SPI and I2C then in the I2C part of code it gets stuck after like 3rd transmit function
2023-04-16 12:44 PM
in main, see if you can get past HAL_Init() or does it go to Error_Handler()?
int main(void)
{
/* USER CODE BEGIN 1 */
uint8_t buf[256];
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
if(HAL_Init() != HAL_OK)
{
Error_Handler();
}
2023-04-16 12:46 PM
it doesnt go to error handler
2023-04-16 01:00 PM - edited 2023-11-20 08:05 AM
why is sys-clk-config light grey ?
2023-04-16 01:06 PM
how about removing all your peripherals you've added, SPI, I2C, TIM2. See if your RB11 or RA15 toggles
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_15);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
2023-04-16 01:07 PM
no idea actually, seems normal to me in the editor. I changed theme to black now to see the difference but they all look the same either way
2023-04-16 01:10 PM
I created a new project and pasted your code in and it's the same. doesnt work :/
2023-04-17 12:25 AM
this CANNOT be wrong...
what you use: custom board or disco ..?
2023-04-17 12:26 AM
it's a PCB that I made, using STM32L431CCT6