cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_CAN_Transmit behavior for CAN Bus OFF

krishr
Associate III

Hi,

When i use HAL_CAN_Transmit to send a CAN message on STM32F4, if say I am in error passive or bus off condition, what error does the API return? If I am in error passive, what is the best way to reset the error count to 0?

Where can i get the error flags related to this as the HAL_CAN_Transmit does not return the error status such as passive or bus off?

There are only two nodes on the bus.

Thanks in advance!

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

Each time you have a question, it's recommended to first refer to the documentation either the reference manual or the datasheet.

In your case you need to refer to RM0090:

Figure 345:

SofLit_0-1720636072735.png

Page 1108:

SofLit_1-1720636188592.png

As you see TEC and REC counters are read only bits. So you can't reset them by software but you need conditions described in the CAN standard to reset them.

See for example this link https://www.csselectronics.com/pages/can-bus-errors-intro-tutorial#:~:text=Specifically%2C%20every%20CAN%20node%20keeps,if%20the%20TEC%20exceeds%20255

Especially the section CAN node states & error counters

SofLit_0-1720646594912.png

But as you have errors with only two nodes you need to check your hardware, your tranceiver, its power supply, your wiring, what about terminating resistors ? do you have any EMI issues? see this link.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
mƎALLEm
ST Employee

Hello,

Did you set the Automatic bus-off ?

SofLit_0-1720632625468.png

i.e.:

CanHandle.Init.AutoBusOff = ENABLE;

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thanks for your reply, AutoBusOff is enabled. There are only two nodes on the bus and after some period of time (say days), one node is going into error passive (say when TEC exceeds 128). So when the other node requests some data, the second node is not able to respond for a long period of time. This leads to a communication loss. I wanted to know how to reset the error states in such conditions.

Hello,

Each time you have a question, it's recommended to first refer to the documentation either the reference manual or the datasheet.

In your case you need to refer to RM0090:

Figure 345:

SofLit_0-1720636072735.png

Page 1108:

SofLit_1-1720636188592.png

As you see TEC and REC counters are read only bits. So you can't reset them by software but you need conditions described in the CAN standard to reset them.

See for example this link https://www.csselectronics.com/pages/can-bus-errors-intro-tutorial#:~:text=Specifically%2C%20every%20CAN%20node%20keeps,if%20the%20TEC%20exceeds%20255

Especially the section CAN node states & error counters

SofLit_0-1720646594912.png

But as you have errors with only two nodes you need to check your hardware, your tranceiver, its power supply, your wiring, what about terminating resistors ? do you have any EMI issues? see this link.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you for your reply. I will check the points you have explained and revert.