cancel
Showing results for 
Search instead for 
Did you mean: 

H750 USB Host enumeration after reset

Pedro3
Senior

Hello!

I'm facing an odd problem with STM32H750VB MCU and the USB Host routine on a custom board. I'm working with the latest HAL (v1.11.2) at 400 MHz and USB using the 48 MHz internal RC, "host only" mode + FatFs "read-only". The software is quite simple: it detects a flash drive, mounts it and try to open a text file. If so, the file is closed, the flash drive is unmonted and then, the board is reset by "HAL_NVIC_SystemReset".

 

The issue lies on this: after the board reboot with the flash drive still connected to the USB, the software detects it but doesn't enumerate it. It waits up to 30 seconds for the enumeration and then, a new reset is triggered, After that, it works! Keeping it cycling, the 1st reset works, the 2nd reset don't, the 3rd reset works, the 4th don't, and so on... Within this 30 seconds waiting, if I remove the flash drive from USB and plug it again, works flawless.

 

Do you guys have any ideia about this behavior? I also tried to "DeInit" the USB host and disabled USB voltage detector before the reset, without success.

 

Thanks a lot!

2 REPLIES 2
FBL
ST Employee

Hi @Pedro3 

Would you share a minimum of your code ? You may miss proper de-initialization of the USB host before resetting the board.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @FBL, thanks for your response.

 

Sure, I can share the code but just to let you know, before calling "HAL_NVIC_SystemReset", I tried to call "MX_FATFS_DeInit", then "MX_USB_HOST_DeInit" and finally "HAL_PWREx_DisableUSBVoltageDetector". Even add a 100 ms delay before the reset...