cancel
Showing results for 
Search instead for 
Did you mean: 

H7 power dissipation and lifetime, how to manage?

regjoe
Senior II

Hello,

I came across this document here https://www.st.com/resource/en/application_note/dm00622045-stm32h7-series-lifetime-estimates-stmicroelectronics.pdf

We have a H75x custom board running the MCU in VOS1 at 400MHz with external 1.2V core power supply.

According to this description here

According to Figure 2, when VOS1, VDD = 3.3 V, VCORE = 1.2 V and operation ratio of 100%. Some examples are
illustrated such as:
• Tj = 105°C the lifetime estimation is > 10 years
• Tj = 125°C the lifetime estimation is 4 years
• Tj = 140°C the lifetime estimation is 2 years
In the same conditions and for an operation ratio of 20%, the lifetime estimation is as following:
• Tj = 125°C the lifetime estimation is 20 years
• Tj = 140°C the lifetime estimation is 10 years

the power consumption, heat dissipation and lifetime is influenced by "operation ratio". What does operation ratio mean and how can I influence/control it? Does this mean that only a part of chip silicon is powered/used? Or time spent in the idle loop, assuming the MCU is running in lowest VOS mode and/or clock frequency during idle time?

Thanks,

Jochen

 

 

 

 

 

 

21 REPLIES 21
LCE
Principal II

This is the first time I ever heard about limited uC lifetime.
> This made me wonder if newer ST uCs are less reliable if running at nominal CPU speed.

Same here! :D

Second I try to measure the CPU load... 

And I wonder if that is the only problem - how much does it "help" for longevity if the CPU sleeps, but DMA & peripherals are running in parallel ? Even though these usually run at 1/2 SysClock.

RTOS: I'm sure these have some "sleep" states ?

Measurement: the M7 ARM has the very accurate cylce counter "CYCCNT", incrementing with each CPU clock cycle, which is probably the most accurate internal tool for timing measurements.

I use it together with a 1 ms SysTick.

/* +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* CPU cycle count activation for debugging */
	CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk;
	DWT->LAR = 0xC5ACCE55;
	DWT->CYCCNT = 0;
	DWT->CTRL |= DWT_CTRL_CYCCNTENA_Msk;
	DWT->CTRL |= DWT_CTRL_PCSAMPLENA_Msk;

/* for accurate measurements, disable IRQs 
 * and use memory barriers */
__DSB();
__disable_irq();

	u32CycStart = DWT->CYCCNT;

source code to be tested

	__DMB();
	__DSB();
	u32CycStop = DWT->CYCCNT;

__enable_irq();

 

I'm not sure which memory barriers (ISB, DMB, DSB) are really required - but it makes a difference to use some at all. I recently checked some multiplication vs bit shift speed, and without the memory barriers the speed was unrealistically low (factor of 4).

 

Ozone
Principal III

>> This is the first time I ever heard about limited uC lifetime.
>> This made me wonder if newer ST uCs are less reliable if running at nominal CPU speed.

> Same here! :D

Not for me.

Especially when the Pentium-4 raised PC power requirements to insane levels about two decades ago, heat-related failures became more frequent. And besides the exploding LV supply rail caps, processors began to suffer from "heat strokes" and related damages as well. Most modern processors, especially not of the x86 kind, would survive an hour without thermal throttling.

And high-end MCUs like the H7 are moving into this direction - and will eventually need to take the same precautions.