cancel
Showing results for 
Search instead for 
Did you mean: 

Graphic Library firmware

stefanoroggerini9
Associate
Posted on June 01, 2010 at 10:38

Graphic Library firmware

#unavailable-resources #unavailable-resources #setting-a-bad-example #stm32
19 REPLIES 19
swhite2
Associate III
Posted on May 17, 2011 at 13:53

For the benefit of other forum members here's a link to the document referred to.

http://www.st.com/stonline/products/literature/an/16918.htm

http://www.st.com/stonline/products/literature/an/16918.htm

swhite2
Associate III
Posted on May 17, 2011 at 13:53

If the library was on ST's site it'd expect it to be here

http://www.st.com/stonline/products/support/micro/files/an3128.zip

Since it isn't either it isn't posted yet (the AN is only a few weeks old) or its somewhere else.

Where did you find the original link to AN3128? Its not on the main STM32 download page at

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=110

stefanoroggerini9
Associate
Posted on May 17, 2011 at 13:53

I don't remember , probably I find the document on

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&fam=110

 but now is not here.I'll wait for the zip file.

Regards.

Stefano

cmanzanal9
Associate
Posted on May 17, 2011 at 13:53

Any news regarding source code described by

AN3128

.

pdf

? How to get the library? It seems to have vanished.

Microchip and

Luminary

Micro provide free graphics libraries. What are the plans of

STMicroelectronics

?

Regards,

Posted on May 17, 2011 at 13:53

Maybe it's another one that you have to specifically request?

See: 

[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/AN2799 - STM32 and STPM01 - Source Code&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/AN2799 - STM32 and STPM01 - Source Code&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E

philippe_chapus
Associate II
Posted on May 17, 2011 at 13:53

Hi All,

I went on a ST seminar in Rousset (France).

They said that this graphics library will be available during 1st quarter of 2011.

You have to wait.

Philippe

Nickname12657_O
Associate III
Posted on May 17, 2011 at 13:53

Dear All,

We are pleased to inform you that the STM32 Embedded GUI library release is now available(attached). Please refer to application note AN3128 for a complete description of the graphical library Objects/API.

The full package contains the STM32 Embedded GUI library and demonstrations firmware as well as a software application Resource Editor (User Interface).

  1. The STM32 Embedded GUI demonstrations are running on the following Evaluation board:  

    • STM3210B-EVAL Board,
    • STM3210E-EVAL Board ( for High density and XL density devices)
    • STM3210C-EVAL board,
    • STM32100E-EVAL Board
    • STM32100B-EVAL Board.

  2.  The software application Resource Editor (User Interface UI) is provided to leverage the feature of the STM32 Embedded GUI Library. This UI allows the user to develop his own screens using the controls provided by the library and then generate the source code (header and c file) which can be integrated in the firmware application. For more details on how to use the Resource Editor please refer to the software help file (after installing the software application).
Cheers,

STOne-32

afinko
Associate II
Posted on May 17, 2011 at 13:53

Great step from STM.

Thanks a lot.

aviramd
Associate
Posted on May 17, 2011 at 13:53

Hi,

Is the Firmware supports working with foreign languages fonts? work with unicode? if yes how?