cancel
Showing results for 
Search instead for 
Did you mean: 

is there a puls out function at stm32f10x ?

mehmet.karakaya
Associate III
Posted on September 25, 2011 at 20:50

is there a puls out function at stm32f10x ?

I mean I set the period and the prescaler of a timer

and it gives out square wave at a pin ?

( I mean without using the timer interrupt )
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ColdWeather
Senior
Posted on September 25, 2011 at 20:54

A timer as a PWM generator. See for instance Manual RM0008 (Doc ID 13902 Rev 12), Capital 15.3.9 on page 368.