Posted on May 17, 2011 at 14:15As you mentioned, in STM3210E: http://www.st.com/stonline/products/literature/um/14220.pdf there is two stage tranzistors to pull-up (T1 and T2 on page 32/48). I made the same on my own hardware design and it work just...
Posted on May 17, 2011 at 14:11Hi Carste, thanks for intensive manual. I will try these steps in few days. However, now I need to chose a wright JTAG emulator, because ulink is not supported by OpenOCD. Any suggestions? The Amontec JTAGkey2 costs 11...
Posted on May 17, 2011 at 13:58>The ''#define MAX_LUN 1'' in file mass_mal.h is a dummy. Instead, modify the variable ''Max_Lun'' in file usb_prop.c. If your project works on NAND and SD both, just change this variable to 0 is enough to make PC sees...