2024-11-05 03:43 PM
Hi,
I use STM32F103C8T6 a GPIO input pin to read a high or low signal from another GPIO output pin, and connect a 3Mohm resistor between two pins, and I notice touching GND with hand will influence the signal status, than I measure the resistance between GND and GPIO pin, it is around 10Mohm. I want to isolate the signal from GND interference, how should I do? I have to keep 3 Mohm resistor. will it be better if connect a capacitor between input pin and GND? or connect a large resistor in between?
Solved! Go to Solution.
2024-11-05 06:06 PM
Hi,
I would NOT recommend using GPIOs, directly, for that purpose.
In electronics, there are many Interface devices, for many purposes. I recommend finding one suitable for your application.
Many MCUs have integrated interfaces, perhaps there is a MCU with a suitable interface for your application...
I hope this helps.
Kind regards
Pedro
2024-11-05 04:51 PM
@ULOK wrote:I have to keep 3 Mohm resistor.
Why??
At that level of resistance, it is to be expected that touching with a hand will be significant!
2024-11-05 05:01 PM
Hi, it is intended for hand detection, but touching GND will also be detected which is surprise. 3Mohm vs. 10(or 6Mohm), I want to increase the resistance to GND so that GND will not influence signal that much.
2024-11-05 06:06 PM
Hi,
I would NOT recommend using GPIOs, directly, for that purpose.
In electronics, there are many Interface devices, for many purposes. I recommend finding one suitable for your application.
Many MCUs have integrated interfaces, perhaps there is a MCU with a suitable interface for your application...
I hope this helps.
Kind regards
Pedro
2024-11-05 07:58 PM
Hi Pedro,
Can you recommend a MCU with such interface? and better have CAN interface too. STM32 series will be good to use. Thank you!
2024-11-06 12:37 AM
look at capacitive touch sensing - many microcontrollers have it built in, and there are also external chips available.