cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO_EXTI

SRAM.11
Associate III

Hi people,

    I just work on a Dali project and trying to learn from the demo library I am getting some error can anyone PLEASE help me how to proceed.

I am trying in STM32G0

I am getting error as EXTI.Instruture undeclared i tried EXTI.Instruct but still its showing error  'NVIC_InitStructure' undeclared 

hOW CAN I DECLARE THAT FUNCTIONS

 

 

 

void receive_tick(void) { // Because of the structure of current amplifier, input has // to be negated actual_val = get_DALIIN(); tick_count++; // edge detected if(actual_val != former_val) { switch(bit_count) { case 0: if (tick_count > 2) { tick_count = 0; bit_count = 1; // start bit } break; case 17: // 1st stop bit if(tick_count > 6) // stop bit error, no edge should exist flag = ERR; break; default: // other bits if(tick_count > 6) { if(bit_count < 9) // store bit in address byte { address |= (actual_val << (8-bit_count)); } else // store bit in data byte { dataByte |= (actual_val << (16-bit_count)); } bit_count++; tick_count = 0; } break; } }else // voltage level stable { switch(bit_count) { case 0: if(tick_count==8) // too long start bit flag = ERR; break; case 17: // First stop bit if (tick_count==8) { if (actual_val==0) // wrong level of stop bit { flag = ERR; } else { bit_count++; tick_count = 0; } } break; case 18: // Second stop bit if (tick_count==8) { flag = NO_ACTION; //enable EXTI EXTI_InitStructure.EXTI_Line = EXTI_LINE_6; EXTI_InitStructure.EXTI_Mode = EXTI_MODE_INTERRUPT; EXTI_InitStructure.EXTI_Trigger = EXTI_TRIGGER_FALLING; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); DataReceivedCallback(address,dataByte); } break; default: // normal bits if(tick_count==10) { // too long delay before edge flag = ERR; } break; } } former_val = actual_val; if(flag==ERR) { flag = NO_ACTION; //enable EXTI EXTI_InitStructure.EXTI_Line = EXTI_LINE_6; EXTI_InitStructure.EXTI_Mode = 'EXTI_MODE_INTERRUPT'; EXTI_InitStructure.EXTI_Trigger = EXTI_TRIGGER_FALLING; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); } }
View more

 

 

 

4 REPLIES 4
TDK
Super User

A search on Github turns on this:

typedef struct { uint32_t EXTI_Line; /*!< Specifies the EXTI lines to be enabled or disabled. This parameter can be any combination of @ref EXTI_Lines */ EXTIMode_TypeDef EXTI_Mode; /*!< Specifies the mode for the EXTI lines. This parameter can be a value of @ref EXTIMode_TypeDef */ EXTITrigger_TypeDef EXTI_Trigger; /*!< Specifies the trigger signal active edge for the EXTI lines. This parameter can be a value of @ref EXTITrigger_TypeDef */ FunctionalState EXTI_LineCmd; /*!< Specifies the new state of the selected EXTI lines. This parameter can be set either to ENABLE or DISABLE */ }EXTI_InitTypeDef;

 

Not sure that'll help if you don't know how to define structures. Where did you get this code anyway?

If you feel a post has answered your question, please click "Accept as Solution".
AScha.3
Super User

Hi,

If you generate the code with CubeIDE , (?)

just define the pins you use for exti and in NVIC choose the INT priority.  Then -> generate code -> and init functions are there.

If you feel a post has answered your question, please click "Accept as Solution".
SRAM.11
Associate III

Yes I found this in drivers but i am not sure why these used

if(flag==ERR) { flag = NO_ACTION; //enable EXTI EXTI_InitStructure.EXTI_Line = EXTI_LINE_6; EXTI_InitStructure.EXTI_Mode = 'EXTI_MODE_INTERRUPT'; EXTI_InitStructure.EXTI_Trigger = EXTI_TRIGGER_FALLING; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); }

 I got is from STM32F1 DALI slave library

waclawek.jan
Super User

This is probably based on SPL, which is an older library no longer supported by ST. There's no SPL for 'G0.

You should try to understand the functionality and then reproduce it on the 'G0, rather than just trying to port it blindly.

JW