2018-12-03 01:00 AM
Hi All,
Here I am doing a task with Atollic Turestudio v9.00 in Windows. In this, the objective is to convert IAR based project into Atollic TrueStudio.
In this, i am getting a lot of linking errors. I checked about the included directories and symbols. Those are fine. I am copying all the header files and source files form IAR directory to Atollic TrueStudio. In this prospect it, showing undefined function, undefined variables etc..
Can you please suggest me a better way to do this task?
Thankyou sir.
2018-12-03 02:55 AM
Perhaps providing a short snap shot of the errors might help in understanding what the linker is missing.
2018-12-05 12:39 AM
Hello sir, Here I am getting an functions are undefined. The header are included. Though the inclusion is done, it showing unknown reference error.
Please tell me a solution..