2019-02-20 7:10 AM
Dear All,
I need to a get a delay of 5 microseconds using STM32F407VG Discovery board.
Is using a timer a good option for this or there is other ways available to solve the problem without using any external library?
2019-02-20 7:23 AM
I looked at this before there seems to be only one function HAL_Delay(); which gives you only milliseconds.
The only way I see is to use
for (int i=1; i<1000; i++)
{}
but you need to find a way to measure how many you need. They way I did is. I connected oscilocope
and I do turn a pin high and low before and after the loop to measure fequency.
HAL_GPIO_WritePin and you use SET and RESET to turn it on and off
2019-02-20 7:26 AM
Is using timer here a good idea?
2019-02-20 7:54 AM
I do not know how you want to implement the times as interrupt ? you could use PWM to get 5 microseconds
then you could use to jump on falling or rising to: and do whatever you need inside.
HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{}
2019-02-20 7:58 AM
I was using a timer and polling to generate a delay of 5 microseconds.
2019-02-20 8:16 AM
I do not think that there is anything in C++ or in HAL drivers
But if you go deeper into assembly languages you could do much more start one time 5 microseconds later etc.
But not something I could help you with. Actually I have sensor which have to be driven with different timers, one delayed 3 microseconds before the other kicks in etc.
I did it with various PWM and combination of external NOR and NAND gates. It works pretty well.
2019-02-20 8:20 AM
I guess you just want 5+ usec delay?
Is this delay triggering HW activity or not?
If it's pure SW, if you are just Waiting for 5+ usec delays you can use a SW delay with NOPs.
The number of loops depends on SYSCLK frequency.
2019-02-20 8:41 AM
#define SetupTime 25
void uSec(int us) {
us=us*(PeripheralBusSpeed/1000000)-SetupTime;
__HAL_TIM_SET_COUNTER(&htim2, 0);
while (__HAL_TIM_GET_COUNTER(&htim2)<us);
}
In most of my applications I set up a 32-bit timer (TIM2) freerunning at bus speed. Then I can use it for any short delays
/* TIM2 init function */
static void MX_TIM2_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig;
TIM_MasterConfigTypeDef sMasterConfig;
htim2.Instance = TIM2;
htim2.Init.Prescaler = 0;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 0xFFFFFFFF;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
unsigned long readusclock(void){
return __HAL_TIM_GET_COUNTER(&htim2)/(PeripheralBusSpeed/1000000);
}
void initusclock(void){
__HAL_TIM_SET_COUNTER(&htim2, 0);
}
2019-02-20 9:11 AM
See also examples of DWT_CYCCNT usage, this provide nano-second level granularity without using a TIM
2019-02-20 8:36 PM
I have sensor in order to activate that sensor I need to held line low for 5 microseconds.