cancel
Showing results for 
Search instead for 
Did you mean: 

Generate variable duty pulse immediately upon receiving external event.

SoftHard-dev
Associate

I need to generate a pulse which is activated high immediately by rising/falling input signal around 100Hz with varied width.  I have tried One Pulse Mode and Gated Mode on STM32f334R8T6 so far but none of them were successful. Even I tried on HRTIM, but I did not get how to generate a pulse with determined width after receiving an event.

The image below shows the problem. I appreciate any help in this regard.

 

0 REPLIES 0