2024-11-30
02:42 AM
- last edited on
2024-12-02
12:09 AM
by
Maxime_MARCHETT
The serial port 1 code generated by the latest STM32CubeMX 6.13.0 will print garbled characters, and using the serial port routine UART_Printf in STM32Cube_FW_H7_V1.12.0 will also print garbled characters.
It doesn't work when using the serial port routine UART_Printf in STM32Cube_FW_H7_V1.11.2. After comparison, there is a difference here. I can’t understand the function here. I will be careful whether changing it will affect other functions.
*This post has been translated from Chinese to comply with the ST Community guidelines.