2024-08-08 03:03 AM
Hello.
I'm trying to set up filters for std IDs on g431. It works in general, but there's a small problem. If I add a filter with the type "Dual ID" (01 in SFT bitfield), only messages with SFID1 are accepted.
For example: filter element value 0x49050306
Green 11 bit - SFID2 - b01100000110 - 0x306
Red 11 bit - SFID1 - b0100000101 - 0x105
Blue 3 bit - SFEC - b001 - store in fifo0
Yellow 2 bit - SFT - b01 Dual ID filter for SFID1 or SFID2
From RM:
I expect that messages with ID 0x306 and 0x105 will be accepted. But only messages with ID 0x105 are accepted.
There are no problems with other filter modes, everything works.