cancel
Showing results for 
Search instead for 
Did you mean: 

g051 serial problem

kevint1
Associate

Hi

I have made a board using the g051k6 chip. I have not been able to receive data from another board sending data at 115200 bd. I connected another serial port to the input pin , and all data is received without errors. A uart problem is mentioned in the errata. The project was created with the cubeide , and I am using the hal uart receive function. Has anyone else had problems with the g0 uart? Basically I want to know if I should just create a new board with a different cpu, or if there is a simple fix.

Thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Andrew Neil
Super User

Have you put an oscilloscope on the pin to see what's actually happening?

"I want to know if I should just create a new board with a different cpu, or if there is a simple fix."

Impossible to say before you've got a better idea of what's actually going wrong.

You did prototype this (eg, on a devboard) before committing to a PCB design - didn't you?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
waclawek.jan
Super User

Which pin? Which UART? What clock?

You can also try to swap Rx and Tx pins in UART using USART_CR2.SWAP and transmit on the same pin.

JW

Andrew Neil
Super User

"A uart problem is mentioned in the errata"

What problem, exactly?

Does it apply to your use-case?

Would that problem produce the symptoms you are seeing?

Have you tried any workarounds mentioned in the errata?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.