2014-11-23 8:39 AM
STM32F407 datasheet says max fsmc clk = 60Mhz
FSMC_CLKDivision = 2; // 168/2 = 84MhzFSMC_CLKDivision = 3; // 168/3 = 56MhzSo what is CLKDivision for 60MHz? ?? #fsmc-clk2014-11-25 9:58 AM
> STM32F407 datasheet says max fsmc clk = 60Mhz
>
> FSMC_CLKDivision = 2; // 168/2 = 84Mhz > FSMC_CLKDivision = 3; // 168/3 = 56Mhz > > So what is CLKDivision for 60MHz? ?? HCLK is not necessarily 168MHz. If, for example, you set HCLK=120MHz, then you can use FSMC_BTRx.CLKDIV = 2 or above. For HCLK above that, the divider has to be at least 3 and FSMC_CLK will be less than 60MHz. In every case, your synchronous memory has to support that speed. JW