2021-08-03 12:56 AM
Hello
1628027999 should mean 2021-08-03 23:59:59,at least from a website that does not claim to keep in account any time zone,so I guess(wrongly ??)that it is referred to 0° Longitude
rawtime= 1628027999;
gmtime_r(&rawtime_t, &my_tm_struct);it returns correctly tm_year, tm_month,tm_day ,tm_min,tm_sec.
I notice that tm_hour is 21 ,instead of 23 as expected.
The only way I found to get what i figure as correct is to increase rawtime before calling function
rawtime + =7200;//seconds in 2 hoursIt's me acting wrong or what else?
I did not add any longitude data.
Is my patch legit?
Thanks for answers,hints or reading.
PS anyway the purpose is to fill other kind of struct :
RTC_TimeTypeDef and RTC_DateTypeDef to load an RTC on a STM32Lxx device
2021-08-03 6:24 AM
1628027999 is August 3, 2021 21:59:59 UTC.
JW