2023-01-18 03:45 AM
2023-01-18 04:57 AM
Hi @IdV,
I'm not sure but first thing coming to my mind is the project setting in your IDE. Have you included the DSP library?
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-18 05:34 AM
Hello, Thank you for your answer. Figure 1. STL architecture says there are no dependencies to a DSP library. So I have that not included this library. But this is necessary to PASS the tests?
2023-01-19 06:32 AM
@JHOUD I have included the dsp lib, but still fails on TM9
2023-01-19 06:47 AM
Hello @IdV, is this self-test on of ST examples? Or a third party? I can try to see myself, but I need a link to the code.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-24 05:00 AM
@JHOUD , ICan you please tell me which functions of the microcontroller fall under the dsp functionality. What does this TM9 test? maybe I'm not using dsp functionality at all, so I can disable the test.
2023-01-30 03:07 AM
I don't know what's the origin or purpose of this TM9 test. I don't think it's coming from ST, probably some third party.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.