Flickering in Dynamic graph widget of TocuhGfx
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-06-29 10:01 AM
Hi All,
I am working on a Dynamic graph widget on the STM32F7 board. Below is the configuration of my setup.
1. Controller: STM32F756ZG
2. Display: Waveshare 7" LCD with 800x480 resolution
3. External RAM: SRAM 8 MByte
I have attached the project and video for reference. Currently, I have not used RTOS and TouchGFX_process is called from the while loop.
Labels:
- Labels:
-
STM32F7 Series
0 REPLIES 0