2012-08-21 11:21 AM
Oh, thats a really nice idea. I'm running 168 Mhz so i have 5 wait states for the flash.
But unfortunately i have no idea if i'm running from flash or ram.I used the standard settings from Crossworks IDE. If I compile the project there are 4.8 kb of flash used and 0.2 kb ram. I suppose it runs from flash? And I would be really glad if you could explain the pipeline thing to me. I basically know what pipeline is from university, but i did'nt get it.Thank you for your help!