cancel
Showing results for 
Search instead for 
Did you mean: 

Flash Erase operation

VKuma.10
Associate II

Hi I'm usiing STM32F746 controller, I am erasing sector 7 using HAL_FLASHEx_Erase(FLASH_EraseInitTypeDef *pEraseInit, uint32_t *SectorError).

Erase operation is successfull but the Controller functionality is not working i.e it is not taking any inputs and not delivering any output

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Bowman32
ST Employee

Hi @Community member​ 

"but the Controller functionality is not working i.e it is not taking any inputs and not delivering any output" Can you please specify when the MCU is not responding?

Bouraoui

Thanks for the reply Bouraoui....

As soon as the Erase operation performed on sector 7 the MCU stops responding .​

I am using sector 7 to store some data ​because it is free.

Is there any problem if I use free memory in flash?​

Hi @Community member​ 

During the erase operation the CPU is stalled.

Bouraoui

I think the Data Sheet should indicate the min/max times for various Flash Sector erases, depends on size and age, as well as voltages.

To avoid stalls during erase and write operations you would need to move the entire working set of code to SRAM

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Even after erase operation is completed code execution is not started How can i restart the execution of code after erase operation