cancel
Showing results for 
Search instead for 
Did you mean: 

FLASH_CR address

PMerc.1
Associate II

Hi,

I am developing a programmer over the SWD and need some advise. One of the tasks is to unlock the Flash with the unlock bit in the FLASH_CR register. I have found a reference manual and it says the offset is 0x10 but I can't find anywhere which states the base address.

Any assistance would be greatly recieved.

4 REPLIES 4
PMerc.1
Associate II

I should have said the specific device is a STM32F746

Thanks @PMerc.1​ 

Indeed, I can then redirect the post to relevant topic to reach relevant community.

Hope someone can help you further there

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PMerc.1
Associate II

Hi Olivier,

Has this been redirected yet?

Paul

Piranha
Chief II

RM0385, section 2.2.2, Table 1, boundary address, "Flash interface register".