2019-02-18 2:32 PM
Hello,
On latest Atollic TrueStudio version (and at least since v9.0.1) the linker script included in default projects for all STM32 chips that I have tested (L476, F303, L053, F042, F070) are broken and will send the software directly into an infinite loop, preventing the software to actually start.
This affects projects generated via File > New > C Project > Embedded C Project and selecting a chip.
On the other hand, the linker script given by CubeMX is valid.
Would it be possible to fix that ?
(On a side note, this should be tested thoroughly since it gives off a very negative image of the quality of ST products...)
Best regards,
Julien FAUCHER