2020-09-08 3:33 AM
Hello,
I'm trying to debug an custom board with STM32L010C6 and STLINK V2. The firmware download seems to work fine, but the debugging is not working. The execution stops here:
0x1FF00220 4800 LDR r0,[pc,#0] ; @0x1FF00224
I've already tried to break at SystemInit() and main(), but they are not reached.
It seems to be a problem in my board, because the same project works fine debugging on a Nucleo MCU, but I cannot yet figure out the problem.
I'm working with Keil uVision 5.31.0.0
¿Any ideas please?
Thank you
Solved! Go to Solution.
2020-09-08 5:48 AM
I already figured out the problem, Boot0 was not properly connected to ground.
2020-09-08 5:48 AM
I already figured out the problem, Boot0 was not properly connected to ground.