2019-06-01 06:03 AM
I'm using STM32L496 discovery board and spi nand flash memory..
i'm trying to use uffs file system ...
is there any porting documentation available for uffs file system into spi nand flash???
2019-06-01 06:24 AM
Sure there are docs and examples if you look for them. Most everything can rather generic so don't make it "STM32" specific. There are SPI transport examples in the NUCLEO BSP, and others.