2022-12-26 04:15 AM
In any mode of FDCAN, receiver doesnot seem to be working. My project is attached.
.
2022-12-27 06:37 AM
Thanks @Community member & @Imen DAHMEN
After connectivity check, it worked. But few observations:
1) Fdcan receive handler not functioning smooth as it stucks after 3 messages & large delay is being observed.
I am using the example code.
2) Can i set my clock to HSI 16 MHz ... as i tried changing it to HSI(16 MHz) from PLL(64 MHz) & setting bit parameter accordingly, fdcan was not seen working.
Pls reply on above.