cancel
Showing results for 
Search instead for 
Did you mean: 

FDCAN Configuration on STM32H723ZGT6

Aashritha_Vuda
Associate II

Hi all,

I am configuring FDCAN3 on the STM32H723 to receive data for a specific ID, but I'm encountering an issue. Here's what I've done so far:

We have configured the FDCAN filter as follows:

 

 

Filter_config_def.IdType = FDCAN_STANDARD_ID;
Filter_config_def.FilterIndex = 0;
Filter_config_def.FilterType = FDCAN_FILTER_MASK;
Filter_config_def.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
Filter_config_def.FilterID1 = 0x7E8;
Filter_config_def.FilterID2 = 0x7E8;
Filter_config_def.RxBufferIndex = 0;

 

 

Then, we applied the filter using:

 

 

if (HAL_FDCAN_ConfigFilter(&hfdcan3, &Filter_config_def) != HAL_OK) {
Error_Handler();
}

 

 

However, I am still receiving all IDs, such as 0x90, 0x7E8, and 0x110, even though I only expect 0x7E8. I would like to call the callback function only when data with ID 0x7E8 is received.

Here is the relevant configuration for FDCAN3:

 

 

hfdcan3.Instance = FDCAN3;
hfdcan3.Init.FrameFormat = FDCAN_FRAME_FD_NO_BRS;
hfdcan3.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan3.Init.AutoRetransmission = DISABLE;
hfdcan3.Init.TransmitPause = DISABLE;
hfdcan3.Init.ProtocolException = DISABLE;

hfdcan3.Init.NominalPrescaler = 50;
hfdcan3.Init.NominalSyncJumpWidth = 1;
hfdcan3.Init.NominalTimeSeg1 = 2;
hfdcan3.Init.NominalTimeSeg2 = 2;
hfdcan3.Init.DataPrescaler = 1;
hfdcan3.Init.DataSyncJumpWidth = 1;
hfdcan3.Init.DataTimeSeg1 = 1;
hfdcan3.Init.DataTimeSeg2 = 1;

hfdcan3.Init.MessageRAMOffset = 0;
hfdcan3.Init.StdFiltersNbr = 1;
hfdcan3.Init.ExtFiltersNbr = 0;
hfdcan3.Init.RxFifo0ElmtsNbr = 2;
hfdcan3.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan3.Init.RxFifo1ElmtsNbr = 1;
hfdcan3.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan3.Init.RxBuffersNbr = 1;
hfdcan3.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
hfdcan3.Init.TxEventsNbr = 1;
hfdcan3.Init.TxBuffersNbr = 1;
hfdcan3.Init.TxFifoQueueElmtsNbr = 2;
hfdcan3.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
hfdcan3.Init.TxElmtSize = FDCAN_DATA_BYTES_8;

 

 

Any insights or suggestions on how to configure the filter or callback to only process messages with ID 0x7E8 would be greatly appreciated.

Best regards,

Aashritha

4 REPLIES 4
SofLit
ST Employee

Hello,

First you need to describe what the issue is:


@Aashritha_Vuda wrote:

Hi all,

I am configuring FDCAN3 on the STM32H723 to receive data for a specific ID, but I'm encountering an issue.


Second, please use </> button to paste your code. I'm editing your post.

Third, this post was posted in STM32CubeIDE which doesn't have any relation to the IDE. Needs to be moved to STM32 MCU products (linked to the MCU usage).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
SofLit
ST Employee

After editing your post, I've noticed the description in the middle. That's why you need to use </> button for the code.

Try this

Filter_config_def.FilterType = FDCAN_FILTER_MASK;
Filter_config_def.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
Filter_config_def.FilterID1 = 0x7E8;
Filter_config_def.FilterID2 = 0x7FF;

+

  HAL_FDCAN_ConfigGlobalFilter(&hfdcan3, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE);

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
SofLit
ST Employee

Another remark:

Avoid this kind of timing configuration:

hfdcan3.Init.NominalPrescaler = 50;
hfdcan3.Init.NominalSyncJumpWidth = 1;
hfdcan3.Init.NominalTimeSeg1 = 2;
hfdcan3.Init.NominalTimeSeg2 = 2;
hfdcan3.Init.DataPrescaler = 1;
hfdcan3.Init.DataSyncJumpWidth = 1;
hfdcan3.Init.DataTimeSeg1 = 1;
hfdcan3.Init.DataTimeSeg2 = 1;

 Very low TSEG1 and TSEG2 values.

You can use this link for CAN bit time calculation to select the suitable values of TSEG1 and TSEG2.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
ahsrabrifat
Associate

Check if you have enabled the interrupts for the FIFO.